Part Number: CSD18513Q5A Other Parts Discussed in Thread: CSD18543Q3A Dear TI,
could you please give us 100% lead free alternatives for the following items:
CSD18513Q5ACSD18513Q5AT
They have 7a exemptions.
Thank you
Part Number: LM3150 Other Parts Discussed in Thread: CSD18513Q5A , CSD18563Q5A We are currently using the LM3150 to convert 24 V to 5 V and a seconden one for 24 V to 12 V. Normaly we are using the CSD18563Q5A as MOSFET 1 and 2. Unfortently this MOSFET…
Part Number: LM5177 Other Parts Discussed in Thread: CSD18513Q5A Hello,
We are using the LM5177 Buck-Boost converter to convert a 10–30V input to 18V / 12A output, but we are facing an issue where the output voltage is only 0.6V.
During debugging…
Part Number: LM25145 Other Parts Discussed in Thread: CSD18513Q5A , LM5145 I cannot understand why there is the need to used different mosfets for the high and low side.
1. All application examples and webench configurations use different but very similar…
Part Number: LM34936 Other Parts Discussed in Thread: CSD19502Q5B , CSD17303Q5 , CSD18513Q5A
Hi,
We are considering the circuit configuration shown in the attached image. Could you please check if there are any problems with the constants of the peripheral…
Part Number: LM74610-Q1 Other Parts Discussed in Thread: CSD18513Q5A There is a request for a schematic review from a customer.
- The input reverse polarity protection circuit is configured by applying LM74610-Q1. (Case 1.)
- Use 2 motor drivers …
Hi Sagar,
Thanks for your inquiry. I am the applications engineer for TI's power MOSFETs. I'd recommend at least a 40V FET for 28V maximum input voltage. For 40V in a 5x6mm SON (QFN) package, the best cost/performance tradeoff is the CSD18514Q5A. For…
Part Number: LM25117 Other Parts Discussed in Thread: CSD18513Q5A Tool/software: WEBENCH® Design Tools I am working on a design using the LM25117.
The circuit seems to be working OK, my prototype boards are working and the regulator is able to produce…
Part Number: 66AK2G12
Hi
My customer will design power supply using IC discrete for 66AK2G12.
Can I use the attached block diaglam?
Or are there the reference circuit designed IC discrete?
66AK2G12 Power supply.pdf
Best regards,
Y…