Part Number: PSPICE-FOR-TI Other Parts Discussed in Thread: LM5109B , CSD18532KCS Why do so many TI FETs fail to converge in Pspice for ti.
Got a simple simulation with a LM5109B driver chip. All the fets in the "Pspice" library run just fine (IRFxxxx…
Part Number: LM5088 Other Parts Discussed in Thread: CSD19502Q5B , CSD18532KCS , CSD18542KCS Hi ,
I am in the design stage of DC-DC 18VDC/7A Board with the use of LM5088 IC. As per the Reference circuit provided by TI, the suggested Mosfet M1 part No…
Part Number: TIDA-00120 Other Parts Discussed in Thread: CSD18532KCS , CSD18502KCS , UCC27211 , CSD18502Q5B , CSD18532Q5B , CSD17581Q5A , CSD18540Q5B , CSD18531Q5A I am trying to implement a slightly different version of the TIDA-0120 charge controller…
Part Number: LM74670-Q1 Other Parts Discussed in Thread: TIDA-00858 , CSD18532KCS , , LM74700-Q1 , TLV1805 Hello,
I am designing a LLC resonant converter with output rated at 3.5kW/ 28V. Since the current drawn from load is around 120A, even the rectifier…
Natallia,
The CSD18532Q5B is not auto qualified. However, it is qualified for industrial applications and rated up to 150degC.
If the customer does not require Q1, do you know what temperature they want it rated to? If they want 175degC, would they…
Other Parts Discussed in Thread: CSD18503KCS , CSD18532Q5B , CSD18534Q5A , CSD18532KCS I want to evaluate NexFET for synchronous rectification, but the provided SPICE models don't work in Orcad Capture 16.3.
Initially, I put the NexFET SPICE model in…
Dear Sir,
Please find attached the captured waveform showing 5–6 cycles of the line voltage and the scaled-up line current.
I have used the same reference design PMP11064 for testing. The current test conditions are Vout = 20 VDC and Iout = 1…