Other Parts Discussed in Thread: CSD18541F5 Hi, in the table 3 the Iout_max is calculated as 21mA using the formula Pmax/Vds_max =0.5/23 = 21mA.
In the datassheet of the M1 mosfet used in Figure 2 (CSD18541F5) the Vds_max is 60V and not 23V as stated…
Part Number: CSD18514Q5A Other Parts Discussed in Thread: CSD18541F5 Hi Team,
We did not find the ESD data of CSD18514Q5A i n the datasheet.
Can you provide?
Best Regards
James Man
TI Customer Support Center
Part Number: CSD18532KCS Other Parts Discussed in Thread: CSD18543Q3A , , CSD18541F5 Hi Team,
A customer would like to amplify a 3.3V PWM signal into a 36V PWM signal.
Can you suggest the right device for the following requirements?
In: 300kHz…
Part Number: CSD19532Q5B Other Parts Discussed in Thread: CSD18543Q3A , CSD18541F5 , UCC27531 , UCC27614 , UCC57108 , CSD19538Q3A Tool/software: Hello everyone;
System Supply Voltage 48V;
We are working on robot actuator series.
We use solenoid…
Other Parts Discussed in Thread: CSD18541F5 , CSD18543Q3A , CSD19538Q3A , CSD88539ND , CSD19538Q2 Hi,
I have a query regarding selection for PMOS, NMOS, or complementary mosfet.
Requirement is to find mosfets for the switching of 500KHz frequency…
Other Parts Discussed in Thread: CSD18541F5 , CSD17483F4 Hello,
My customer is searching for a FET which can be used for CCLD(Constant Current Line Drive). It seems it is also called as IEPE, ICP, Delta Tron and so on depending on the equipment makers…
Hi Wesley,
Thanks for the inquiry. Unfortunately, we do not have a pin-to-pin replacement for the LBSS139DW1T1G dual NFET. The customer could use 2 of the CSD18541F5 single NFETs. Please keep in mind, the rds(on) of this device is orders of magnitude…
Part Number: DRV8323 Other Parts Discussed in Thread: CSD18541F5 , Hi,
we are using the DRV8323 to drive small MOSTETs type CSD18541F5 in 3x PWM mode to control a small 24V-BLDC motor (motor power 9W). See schematics below. If the PWM input is either…
Hi Narayan,
Thanks for the inquiry. A short from drain to source is a very typical failure mode in a MOSFET. There are many possible causes. Without knowing more about the application, it is difficult for me to determine why the FET may have failed…
Part Number: PMP22504 Other Parts Discussed in Thread: CSD18541F5 , CSD88539ND , LM74610-Q1 HI Expert,
about the ideal bridge diode, could you help to check if we can replace the NMOSFET – CSD88539 by CSD18541*2 to save some board space? Thanks. …