Part Number: CSD88539ND Other Parts Discussed in Thread: CSD88537ND , Hello team,
There are no specific HBM and CDM level in CSD88539ND, CSD88537ND datasheet.
Would you please help me to get information?
Other Parts Discussed in Thread: CSD88539ND Tool/software: Hi all,.
We are considering using this FET as an alternative to the Renesas HAT2114RJ.
[Conditions]
After the FET is turned on, a reverse electromotive voltage is generated for 17 μs.
…
Part Number: CSD88539ND Other Parts Discussed in Thread: CSD17318Q2 , , CSD85301Q2 Tool/software: HI
We are using LTC4365IDDB#TRMPBF in our design for over voltage and undervoltage protection.We require to choose external Dual Mosfet for a Vin of 5V…
Part Number: CSD88539ND HI Folks,
I am working on a Cadence PsPice simulation examining the Vds voltage drop at 1A and other design parameters, I am looking for a spice model to incorporate in my design. After looking online I do not see a model for…
Part Number: CSD88539ND Other Parts Discussed in Thread: CSD18543Q3A , CSD17577Q3A , CSD17308Q3
Dear community,
I would like to use a dual MOSFETS SOIC such the CSD88539ND for an application which creates a boost converter from +3V to +12V on the…
Part Number: CSD88539ND Other Parts Discussed in Thread: CSD87333Q3D Hi Team,
For Vds:30V have SOIC-8 package?
Spec need similar VISHAY SI4816BDY-T1-GE3
73532.pdf (vishay.com)
Part Number: DRV8711 Other Parts Discussed in Thread: CSD88539ND , CSD88537ND I use DRV8711 with IRF7351in custom board (motor current up to 5A, supply voltage up to 48V). Then i try change mosfet to CSD88539ND in same board, but now I am constantly getting…
Part Number: CSD88539ND The data sheet refers to the case temperature in multiple places, but I cannot find the Theta-J Case specification. Is this available?
Thanks,
Stuart
Part Number: CSD88539ND I have a 4 phase motor but not sure how to determine whether I need a half wave or full wave controller. There are 4 outputs going to the 4 coils in one config so 4 wires and in the other config, in addition there is another output…
Part Number: CSD88539ND
Hello,
Could you tell us about CSD 88539? What is the avalanche (EAR) value under the following conditions? ※ This question is about EAR, not EAS.
VDD = 30 V, Vgs = 20 V -> 0 V, ID = 10 A, L = 100 uH, RG = 25 ohms
Tch …