Part Number: DAC60508 Other Parts Discussed in Thread: MSPM0L1306 Hi,
I want to configure the DAC60508 via SPI on the MSPM0L1306. Looking at the DAC60508 website, it seems that there is no sample code released to do the configuration on TI's MCU, is…
Part Number: DAC60508 Tool/software: Hello,
i'm finding the right solution for my application where I need at least 800 ksps out of a DAC.
I know the empirical rule that out sample rate is just the inverse of the settling time, as a maximum value…
Part Number: DAC60508 Tool/software: I have an application that uses 5 daisy-chained DACs (40 total DAC channels). I would like to update all 40 DAC channels then simultaneously update the outputs of all 40 DACs at the same time.
Is that possible…
Part Number: DAC60508 I am using DAC60508ZCRTET on my hardware. I understand that this DAC do not support readback of data. I want to write data to the DAC with error checking enabled. Is it possible to write to this DAC enabling the CRC? Please can you…
Part Number: DAC60508
When use the DAC60508, should be read in upper four bits (15-12 bits) of address 0x01 during use 0010, now reading 1000, some errors, other address output data is normal. since the address is read-only, what is the reason?
Part Number: DAC60508 Other Parts Discussed in Thread: DAC63204 Dear all,
I've got a project in which I used a DAC60508MRTER because I was under the impression that it would start-up mid-scale using the internal reference of 2.5V. I expected 1.25V on…
Part Number: DAC60508 Hi Team,
VDD and VIO same supply 3.3V
CS has 10K to VDD
No MOSI from chip to be able to read
REF to 2.2uF cap to gnd
SPI clk mode 1
after a reset the default register set seems to be enabled thru the SYNC reg addr 02…
Part Number: DAC60508 I'd like to double check if what is the FS voltage would be when VDD = 5.0V, Vref = 2.5V (Internal) (DIV=1) and Gain = 2.
Here is the circuit I have which is the same as the evaluation board.
Thanks,
-CD
Part Number: DAC60508 We are planning to use DAC60508MCRTET with an external Vref REF3325AIRSER but we could not source the ref. part and DAC60508MCRTET is very low in stock.
The DAC has option for internal Vref but I worry that it might not be accurate…