Part Number: DAC63004 Tool/software: Hi,
I am interested in the DAC63004 smart DAC. I have been reading the datasheet trying to figure out how to output a sine wave for a certain frequency. From what I understand there are hard coded slew rate options…
Part Number: DAC63004 Tool/software: The customer wants to design a constant current source with sine wave output, hoping for bipolar output.Can DAC63004 meet this requirement?
Does DAC63004 sine wave output have a DC component.
Part Number: DAC63004 Tool/software: Hi team..
I need to generate 5V and 0V voltage from DAC through SPI interface. I have tested DAC63004-EVM board with the given GUI, everything is working correctly.
Now I have to use custom board having DAC63004…
Part Number: DAC63004 Hi TI team,
In post
https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/1211336/dac63204-how-fast-is-the-feedback-on-the-dac63204
You mention " There is a 2us delay for the change on the…
Part Number: DAC63004 Hi,
I'm trying to configure daisy-chain operation, as detailed in the datasheet.
First thing is to set SDO-EN in the INTERFACE-CONFIG. This should cause SDO (the GPIO pin) to output the end of the shift-register.
But I think…
Part Number: DAC63204 Other Parts Discussed in Thread: DAC63004 , Hello,
Can the DAC63 2 04RTER and DAC63 0 04RTER be used interchangeably without modifying firmware, or are there functional differences between the two that prevent this?
Thank you…
Part Number: DAC63004 Other Parts Discussed in Thread: TPS7A8300 , TPS7A90 , , DAC63002 , INA296A , OPA186 , TMUX1113 , OPA3S328 , TLA2518 good morning,
I need to develop an analogue board that allows me to accurately vary the voltage between 0.8V…
Part Number: DAC63204 Other Parts Discussed in Thread: DAC63004 , , ENERGIA , DAC53204 , ADS7953 Hi,
I want to "marry" DAC with NVM and multi-channel ADC on one SPI interface.
For this one of them should respond on first data package (? bit) and other…
Part Number: TCAL6408 Other Parts Discussed in Thread: DAC63004 ,
Tool/software:
Hi TI,
It is not a question but a suggestion. Why do not you allow for four I2C addresses instead of just two? Additional two addresses could be easily handled the…
Part Number: DAC63004W Other Parts Discussed in Thread: DAC63004 , DAC532A3W , AFE532A3W Tool/software: Hello TI community!
I am wondering if there are .c, .cpp and/or .h libraries for I2C communication available for this part that I can include in…