Part Number: DAC7311 Hello,
As the title says i am looking for a shift register to use for a simulation on TINA TI.
The reason i'm looking for this is because i am having issues with the SPI signal generator and want to force some values on a DAC7311…
Gerard,
Thank you for the inquiry. The DAC7311 models are encrypted, and for some reason that is confusing the model editor. I will check with the models' originators and then let you know how we will move forward.
Regards, John
Part Number: DAC7311DAC7311IDCKRG4
DAC8311IDCKRG4
Could you please help to confirm if the above parts with G4 suffix are legacy part numbers used during RoHS conversion.
Part Number: DAC7311
Hi Team,
DAC7311 is used for RF signal, but the output has high frequency harmonic which has bad effect on RF performance.
DAC7311 is powered by a 3.3V LDO and the output is set to 0.9V, the frequency spectrum of power supply…
Part Number: DAC7311 Other Parts Discussed in Thread: DAC8411EVM-PDK Hi Team,
MMB0 board is required to work with DAC7311EVM, I cannot find it on TI.com. Could you please tell where to order it? Thanks!
Best Regards!
Hao
Part Number: DAC7311 Other Parts Discussed in Thread: OPA277 Hi,
Our customer evaluated the DAC7311, but the output rail was Vs-0.6V. The circuit and data are below. 1) Are there any problems with the circuit? 2) When the load of the DAC is OPAMP, what…
Part Number: DAC7311 Hi,
My customer has a below question:
In datasheet, SCLK need at least 25ns hold-up time, otherwise it is abnormal.
Customer wants to know if the hold-up time is less than 25ns, what output state it will be?
Thanks!
Other Parts Discussed in Thread: DAC7311 Hi,
I was wondering if I could use the DAC7311 with the NSYNC pin hard connected to GND and just exercising the CLK and DIN pins.
Thanks,
Viktor.
Hello Richard,
As Tony suggested in an older post, the max spec parameter is not included in final test for the DAC7311 device, therefore we may not have data to suggest a max or provide a histogram. I will check with design and characterization to…