Hi,
Please have a look at the DAC81404EVM user's guide schematics. EVM schematics has all the values and designed for 100mA load capability.
https://www.ti.com/lit/pdf/slau825
After going through the same, if you need more help, please post it here…
Anbu, I have verified that pins 1 and 4 of J17 are 5.0V and all others are at ground. We went ahead an ordered another DAC61402 eval board thinking that perhaps the board was damaged through ESD or handling. I connected the new eval board to the Launchpad…
Hi Avi,
Please use this link for the DAC81404EVM GUI. I do not see a DAC61402 GUI published in GUI Composer. The DAC81404 has the same registers, but the two output channels for the DAC61402 are labeled as DACB and DACC in the DAC81404EVM GUI. https:/…
Other Parts Discussed in Thread: DAC8822 , DAC11001A , MSP432E401Y , UNIFLASH , DAC81404EVM Hi,
I am looking for a DAC chip with at least 2 channels, >1M sampling rate, >= 18V output.
Can anyone give some recommendation?
thx.
I so far have managed to use UniFlash app to update latest firmware to the MSP board.
However, when I try to use EVM GUI app to work with the DAC evaluation board, I get stuck.
This post ( BP-DAC81404EVM/BP-DAC61402EVM GUI runtime error - Data converters…
Hello,
The SPI frames will need to meet these timing requirements:
The G431 should work without the gaps that the Uno has as long as the SCLK low and high times are being met. From what I can see in your scope shots, it looks like most of the requirements…
Hi Tom,
We have some EVMs that use a TI Launchpad controller, which could be used for this application. We do not have any ready-to-use APIs or support libraries to automate our EVM functions, but with the flexibility of a microcontroller you could pretty…
Part Number: DAC61402 Which development boards can be used to control DAC61402 under Linux platform?
The recommended EXP432E401Y LaunchPad and the BP-DAC81404EVM seems can only operate in Windows platform.
Part Number: MSP-EXP432E401Y Other Parts Discussed in Thread: DAC61402 , Hi all, I have ordered MSP-EXP432E401Y LaunchPad and BP-DAC81404EVM integrated with DAC61402, so how to develop MSP-EXP432E401Y with CCS to make it output different voltages? I want to…