Hi Sanjay,
First of all, I would like to thank you for your time and support over call to solve my problem.
Problem: Not Able to communicate with DAC81408.
Summary:
I was interfacing DAC81408 with AM2634 Quad Core Controller over SPI0 and setup to Core…
Part Number: AM2634 Tool/software: Hi Team,
I am trying to interface DAC81408EVM with AM2634. Below tasks are done.
SPI comm from AM2634 to DAC is established
Checked few testcases by setting output voltage to 5V and 10V
Its working for some instances…
Part Number: DAC81408EVM Tool/software: I am having an issue with DAC81408EVM when trying to transmit more than 4 channels to DAC. If I only transmit 4 channels, everything is fine. If I try to transmit more than 4 channels, then the DAC will output…
Part Number: DAC81408EVM Tool/software: Hi Team,
As per out requirement, we need to generate -10V to +10V output from single DAC channel. Is it possible to do that?
If yes then please let us know the configuration setting for the same along with FSR…
Part Number: DAC81408EVM Hello,
I hope this message finds you well. I just want to know that can I connect "DAC81408EVM" board to a microprocessor through Serial/SPI and control it. I do not want to use the software tool in PC.
In advance thank…
Part Number: DAC81408EVM Hello,
We have purchased DAC61408 Eval board, we need to generate negative output from all 8 channels. we have tried connecting Vss to negative 12V.
still no success. we also looked into register configurations.it didn't help…
Part Number: DAC81408EVM Dear Team,
My customer is considering to use the DAC71408 (14-bit), and has the DAC81408EVM and the USB2ANY now. They want to ouput PWL ( Piece-wise Linear) waveform from the DAC81408EVM. For example, a PWL signal source of the PSPICE…
Part Number: DAC81408EVM
Hello Team
I'm trying to control the DAV81408EVM with USB2ANY interface adapter and GUI from DAC81408EVM software downloaded for the TI website.
I use internal 2.5 V reference, Supplying the board with VDD/VAA = 5 V, VCC …
Part Number: DAC81408EVM Hi Experts,
Our customer dac81408 device. However he has no usb2any connector. He is asking if he can use rs232/442/485 as a usb2any device dac810408 EVM?
As far as I know this will not work as the GUI will not work without the…
Part Number: DAC81408EVM
I have been using this DAC-EVM for some time, and all the ports were working fine. Recently I see that THREE out of EIGHT channels are not working.
Channels 02, 06 and 07 are giving voltages -10V, -10V and 10V respectively. My…