Part Number: DAC908 Hi,
For DAC908, in datasheet its mentioned that Output Compliance Range as 1.25V and full scale O/P range is 20mA. Does that mean the O/P current will be limited at 1.25V?
We are using this IC for 0 to 5V trail. Will it work with…
Part Number: DAC908 Hi. How are you?
We're interested in the DAC908 device to generate periodic signals. Something similar to a function generator.
My question is: What is the minimum clock frequency at the CLK pin (pin 28)?
Our idea is to create…
Hi Kris,
We do not have a firmware example for CMOS DACs. Here are some documents that might be helpful though.
5265.Interfacing Data Converters to FPGA.pptx
1055.Interfacing to FPGA's app note.pdf
If you need further assistance, please send me…
Part Number: DAC908 Hello E2E,
Any guidance on specing a transformer for this? I'm driving a single ended 75 Ohm load.
Let me know what additional information you may need.
Russell
Part Number: DAC908 Hi, Is there the IBIS model of DAC908? If Yes, is it possible to have it provided? If No,is there a model similar to IBIS? Best Regards, Yuto Sakai
Other Parts Discussed in Thread: TRF370315 , DAC908 , TRF3705 Hello everybody, I would like to use the DAC908 (one for I and one for Q) as BaseBand inputs for the TRF370315.
At the very beginning I was thinking to ac couple the two devices in order…
Other Parts Discussed in Thread: DAC908 , OPA2690 Hi
My customer plans to use DAC908 with OP Amp to make voltage reference. (1Vmax OUT, variable)
Could you tell me appropriate OP Amps(2ch) for DAC908?
The signal chain block is as below.
DAC908…
Other Parts Discussed in Thread: DAC908 Hi,
i have two questions about DAC908.
1. - What it the output compliance voltage when operating at 3V power? I could only find that it is 1.25V using 5V power.
2 - Can VD and VA power input pins be different…
Dear Specialists,
My customer is confusing the phenomenon of DAC908E's power on.
When the power is on, unexpected output is happened.
Could you please advise me the reason and measures
In detail, please see attached file.
5226.question about…
Part Number: AM5706 Hello,
My customer designs a time-of-flight system around our DAC908 . As they need a high DSP performance and a cycle-accurate control over the DAC and ADC interfaces, we are thinking of the AM5706 and to leverage the 2 PRU-ICSS…