Other Parts Discussed in Thread: DCH010505S Since DCH010505S and DCV010505P passed UL60950 and UL1950, Acbel asks us to provide the related document for UL60950 and UL1950.
Please kindly help check if you have these two document that can share to customer…
Part Number: EK-TM4C1294XL Other Parts Discussed in Thread: DCH010505S , We need the 3D models to add in our Philips library. the models in any universal format like step file.
DDR TERMINATION MODUL 15A 5V
Switched Supply Unit
PTH05010YAZ…
Part Number: DRV8301-69M-KIT Other Parts Discussed in Thread: DCH010505S Tool/software: Code Composer Studio I have a DRV8301-69M-KIT schematic.
1.I' m wondering why U2(DCH010505S) is used.
2. Why should there be IGND?
Other Parts Discussed in Thread: DCH010505S , DRV8312 , CONTROLSUITE Hi there,
I got a DRV8312EVM base board with a F2806x ISO controlCARD. When I give power supply to both boards for a while, the U3(DCH010505S-isolated DC/DC converter) and U4(ISO1050DUB…
Eli,
An LDO may be used to reduce the 12V for a 5V input to either system. Are the DCH010505S and DCH010512D modules acceptable? Is board space the main consideration for this choice?
Thank you for your response,
Manuel Chavez
Hi Rick,
Thanks for the information. I know that the DRV incorporates a buck converter but I jut wanted know if there is any additional except from that. But, as I can see it uses only that and an isolated DCH010505S which is also supplied from the…
Hello Damith Pavithra
http://www.ti.com/product/DCH010505D
Please refer to the part number for the requirement you have.
I do not have a design showcasing this device but have a design that showcases single output
http://www.ti.com/tool/TIDM-HV…
Hello Tim, thank you for posting.
Here are 2 options.
First; TI has many isolated modules, however Vin range is 4.5-5.5 or 10.8-13.2V.
There isn't a module that works at 7.5Vin.
Step down 7.5V to 5V with a buck, then look at the isolated modules…
Hi Rick,
DCH010505S seem ideal but too much increases the BOM. Maybe the REF02 voltage reference IC powered from motor power supply can be a lower-cost choice?
I can use an XMega uProcessor with internal 10 bit DAC that is better than 4 bit builtin…
Part Number: TMS320F28035 Other Parts Discussed in Thread: CONTROLSUITE , TIDM-HV-1PH-DCAC controlSUITE\development_kits\HV_1PH_DCAC\v1_02_00_00\hardware\r3\TIDM-HV-1PH-DCAC-SCH.PDF
Some problems of about TIDM-HV-1PH-DCAC-SCH.PDF
Design Guide: TIDM…