Thanks, it helped a lot. This allowed me to compile system without problem.
But we found out that while X is running gstreamer ducati plugin doesn't work. After killing X I use it to play video via kmssink. It fails in initialization like here(I attached…
HI Kurt:
thank you for your info.
1. for the inductor pole is single or double, from I understand, both is OK, cause it is deduce from internal current loop with sample hold transfer function. if you simplified the ZOH with first order, then the transfer…
Hi Tim,
To decode an error, follow the process below:
Each error is a 32 bit value. bits 31:16 are the error type. If you take your value and right shift 16, you will get this value. For example, the first error you show is -203685722. Right shift…
Part Number: DRA752 Other Parts Discussed in Thread: PMP , DRA742 , , TVP5158 , OPA362 , TFP410 , TPD12S015 , TLC59108 Tool/software: Linux Hi all,
I use GLSDK 3.00.00.03, custom board. It cannot use modetest and frame buffer (/dev/fb0) does not generate…
Eric,
Make sure pin 49 (SCAN_EN) is always tied to GND. Since you have one working device, I would compare every input between the two parts. This would include power, clocks, SPI, ect... If this does not show you anything, you could swap the two parts…
Hello, Badri
Thanks for your reply.
OK, let me describe the firmware files I tested more specifically.
There are 3 case in my test:
case 1:
There is already file system existing in the NAND flash when we got DVRRDK box.
We got the firmware…
Part Number: TDA4AH-Q1 Other Parts Discussed in Thread: TDA4VH Tool/software: New hardware design for
TDA4AH88TGAALYRQ1
TDA4VH, TDA4AH, TDA4VP, TDA4AP series
I am starting a new design for this Ti SOC.
I have a few questions.
For the DDR4…
Other Parts Discussed in Thread: OMAP3530 , SYSCONFIG , ADS7846 Hi All,
I wonder if anyone could help me with issue. I am currently working on custom board and developing Telit Modem Driver. The MODEM driver is only toggling GPIO line to turn Modem…