Hello:
I information and you give me a link error is not the same.
I try to do the following:
$ strace -o log opkg install dlp-sdk_2.0-r8.0_cortexa15hf-neon.ipk
1768.log.txt
View the log file found that there are several directories not created…
Hi Nikshith,
Please use the below attached files - 8865.txt 2364.txt Rename the above RAW video files from .txt to .yuv (e.g 8865.txt to 1.yuv & 2364.txt to 2.yuv) Create the input raw file combination of black and actual raw video -
cat 1.yuv 2.yuv…
I have followed the steps suggested and i am still facing the same issues with the input , i have added all the plots here for more analysis
comparision_outs.zip.txt
Fullscreen
tidl_importfp32.txt
Download
modelType = 2
numParamBits…
Hello Margarita Gashova:
I use the software:
ti-ezsdk_dm814x-evm_5_05_01_04_demo_binaries.tar.gz
this ezsdk include gstreamer-omx versions was: gst-openmax_GST_DM81XX_00_06_00_00
omx version was: omx_05_02_00_46
and gstreamer was:
https:/…
Part Number: TDA2 Tool/software: TI-RTOS Hello, I'm running the TIDL object detection usecase, and usecase is running fine only with a small problem here:
My original input file is .MP4 with resolution 1920*1080, and I make it to .h264 with resolution…
Hi,
We are using the SK-AM62 E3 revision. Can you please confirm which revision are you testing the HDMI audio?
Shorted the j24 pins. Still HDMI audio is not coming.
Attached the boot logs for you.
Fullscreen
5367.Bootlog.txt
Download…
Brad,
1.- Yes. Take a look at pictures RSTP_IDK_Test_1.jpg.txt, RSTP_IDK_Test_2.jpg.txt
2.- Take a look at picture RSTP_IDK_Test_1.jpg.txt.
I am plugging/unplugging both ports. You can see some traces in a post above with issue in eth2.
3.- The…
Hi Margaritha,
What could be the reason that mdiscalar and hdiscalar elements behaving differently?
One thing I observed that while using mdiscalar element 2 out of 3 frames capturd are full of grains as shown in the snapshot below
yuv file :…