Part Number: DIX4192-Q1 Other Parts Discussed in Thread: DIX4192 Hi, Team:
Can you help to check and advise what's the maximum working Tj for DIX4192IPFBRQ1 and D IX4192TPFBRQ1 ?
My customer Alpine has interested with the part.
Thanks.
Part Number: DIX4192-Q1 Other Parts Discussed in Thread: DIX4192 Hi, I have a couple of quick questions:
1. Problem:
In an application the DIX4192 with input A (audio serial port A - SDINA) and output (DIT - AESOUT) used simultaneously. The input is used…
Part Number: DIX4192-Q1 Other Parts Discussed in Thread: DIX4192 If Port A of DIX4192 is used as I2S slave and only DIT is used to transmit SPDIF data. In this case , should MCLK be synchronized with DSP's CLK.
Is a outside crystal OK for this use…
Part Number: DIX4192-Q1 Other Parts Discussed in Thread: DIX4192 what is the founction of BLS and SYNC?
How should BLS and SYNC used in system?
Please give some examples of utility of BLS and SYNC.
DIX4192 is applied in our system to transfer I2S data…
Part Number: DIX4192-Q1 Other Parts Discussed in Thread: DIX4192
Hi,
Let me confirm about below.
According to datasheet of DIX4192, DIX4192 line receivers may also be driven directly from external logic or line receiver devices with TTL or CMOS outputs…
Part Number: DIX4192-Q1 Hi,
According to datasheet, there is following spec.
* Vth "Differential input sensitivity"
I believe that this spec is for differential, however I would like to know how we can consider in case of Coax.
As you know,…
Other Parts Discussed in Thread: PCM9211 , DIX4192-Q1 , DIX9211 Hi, TI support team
Please recommend a product that supports up to 384kHz sampling frequency with functions similar to the parts below.
part name : CS8406
Thanks.
Regards,
MJ
Part Number: DIX4192-Q1 Other Parts Discussed in Thread: AM5728 , TLV320ADC3101
I'm trying to program DIX4192-Q1 by means of Linux userspace application via SPI protocol. Audio data is sourced to this decoder, passing through following elements: Microphone…
Part Number: AM5728 Other Parts Discussed in Thread: DIX4192-Q1 , Tool/software: Linux I use two audio interfaces DIX4192-Q1 on my customboard, based on sitara am5728. One of them is connected to i2c and second to SPI. But I can't find linux driver for this…
Sam,
The TLV320AIC3104 does not have a DIT built in. It could be connected to one of our DIX4192-Q1 transceivers, but thats about it.
best regards,
-Steve Wilson