Other Parts Discussed in Thread: AM3358 , TPS65910 , DA8XX Hi,
I am trying to boot by SD card, but I am facing below error in Linux Image. (Alst refer attached SDcard & Sysboot setting in Board)
Linux Version:: Linux-3.2.0
Processor :: AM3358
…
"But I am not sure it will solve my problem. I think I have maxed out the system"
You may have, but knowing you are putting essentially 0 for the Vth means that you aren't commutating for maximum torque. Many times with no load you will still hit maximum…
here is my kernel info :
CPSW phy found : id is : 0x282f014 IP-Config: Complete: device=eth0, addr=157.87.41.230, mask=255.255.255.0, gw=157.87.41.1, host=157.87.41.230, domain=, nis-domain=(none), bootserver=157.87.41.124, rootserver=157.87.41.124…
Oleg,
The general instructions to update pinmux and rebuilding board for Processor SDK RTOS is provided here:
The instructions are however more specific to newer devices that don`t use starterware baseline, so I would recommend looking at the following…
Other Parts Discussed in Thread: TVP7002 Dear All: I am trying to let v4l2 capture use a usb camera working on my evm814x board from mistral . The EZSDK I am using is Version5_05_01_04.
My usb camera can support the following format: YUY2(320*240) MJPEG…
Hello,
We are using a dm355 evm board and we want to write large files to a SDHC memory card. The demo board running Linux 2.6.32- rc2- davinci ( argo -project ) and the SD card is used as a block device (/ dev/mmcblk0p1 ) and the host controller use…
Hello,
We are using a dm355 evm board and we want to write large files to a SDHC memory card. The demo board running Linux 2.6.32- rc2- davinci ( argo -project ) and the SD card is used as a block device (/ dev/mmcblk0p1 ) and the host controller use…
As mentioned in my previous post, the encoder doesn't encode and the encode demo locks;
I have the following trace; can someone help me?
Thanks
root@dm6467t-evm:/opt/dm6467/demos# CE_DEBUG=3 ./encode -v tt.264 Encode demo started. Debug started…
Hi ,
I am working on DM8148 EVM ,i am using EZSDK 5.03 .I am trying to develop an OMX application for displaying video simultaneously on HDMI and LCD displays .
I am considering OMX Capture-Encode demo for doing this .
I have connected the OMX…
Hi,
Rex,
I had change the increase the size of dsp1_cma_pool to 0x6000000,now I can load it into dsp,but it willl have mmu error.I debug it with ccs,finding that the edmaInit cause it.
root@am57xx-evm:~# ./dsp-ipc.sh 1 rm: can't remove '/lib/firmware…