Part Number: DLP2021-Q1 Other Parts Discussed in Thread: DLP2021AM263Q1EVM 1.If the device is powered off and the DLP2021 light output matrix is not flipped back before power-off, how many times will the DMD2021 be damaged after use?
2.The socket is…
Part Number: DLP2021-Q1 Other Parts Discussed in Thread: DLP2021AM263Q1EVM Tool/software: 1、Is the DLP2021AFQUQ1 device produced by reflow soldering or by locking onto the PCB board?
2、Is the hot pad area of DLP2021 directly exposed copper on the PCB…
Part Number: DLP2021-Q1 Other Parts Discussed in Thread: DLP2021LEQ1EVM , DLP2021AM263Q1EVM Tool/software: I am using the DLP2021LEQ1EVM evaluation module and I want to receive video data through the MCU, and then send the video data to the SPI FLASH…
Part Number: DLP2021-Q1 Other Parts Discussed in Thread: LP-AM263 , DLP2021AM263Q1EVM Tool/software: DLP2021-Q1: We can't enter the uart boot mode whether the pin value is 1000 or 0001. The progress is always 0 when we run python script to flash SBL and…
Part Number: AM2632-Q1 Other Parts Discussed in Thread: AM2632 , DLP2021AM263Q1EVM Tool/software: we have a new project,now use DLP controller AM2632 and DMD DLP 2021. I have some questions as below: 1、The AM2632 DEMO uses power monitoring of 5V, 3.3V…
Ryan,
The schematics referenced (TIDA080004) were designed for Head-up display application, which needs a photodiode feedback scheme. If you are using for a puddle light, then this is not really necessary. This system can be modified to remove the need…
Part Number: AM2634-Q1 Other Parts Discussed in Thread: DLP2021AM263Q1EVM Dear Champs,
When my customer tried to build SBL_QSPI, they faced build error and it looks the error was caused in openssl command.
Could you please check below error log…