Hi Jacob
You can find the Assembly Drawing ( www.ti.com/.../tidruz8.pdf) and other CAD files on the webpage for the TI Reference Design of the DLPDLCR3010EVM-G2 here: www.ti.com/.../tida-01571
Regards
Azad
Part Number: DLP3010 Other Parts Discussed in Thread: DLPC3478 , DLPA3000 , DLPC3438 , DLPDLCR3010EVM-G2 Hi
I have DLPC3478 and DLPA3000, DLP3010
I see that DLPA3000 can work with DLPC3478 and DLP3010.
So, I tried to use DLP3010EVM firmware with…
Hi Ameya,
Welcome to TI E2E forum.
1) 3D scanner is a whole product, TI develops semiconductor chips that can be used in building a scanner. DLP3010 is one such component in the system. I am afraid we will not be able to provide you the complete list…
Other Parts Discussed in Thread: DLPC3438 Hi, Nadine:
The following link http://www.ti.com/tool/dlpdlcr3010evm
on "Available Version(SW)", I see "DLP LightCrafter 3010 Firmware " and "MSP430 HDMI sample code".
Is "DLP LightCrafter 3010 Firmware…
Hi Thomas,
DLP chipset is a combination of DLPC controller DMD and PMIC. DLP3010 can be use with DLPC3433 (or DLPC3438) controller and DLPA200x and DLPA3000 PMIC.
Depend on the chipset combination brightness will differ (PMIC can provide different…
Hi Yosuke Here is the procedure to update the DLP3010EVM-LC batch file using DLPLCRD-GUI. 1. Go to the Advanced version of the DLP Lightcrafter Display v7.0 GUI. 2. In the Flash Image Update section, select EVM type as DLPDLCR3010EVM. 3. Select the DLP3010EVM…
Hello!
We are doing a project where we are looking to use the Lightcrafter 3010 EVM with our own optics. Are there any CAD files of the whole EVM available? We are looking for the mechanical files not just gerber files for the PCB.
It would also be…
Hello Alexander Chan , the document is DSI Setup and Debugging Guide v1.0 which can be accessed here: /cfs-file/__key/communityserver-discussions-components-files/94/0523.dsi-setup-and-debugging-guide-v1.0.pdf
Regards,
Jason
Hi Lucas,
During Vertical blanking and Vsync we actually recommend being in LP11 mode. Please see the screenshot and document attached below for more information.
Best,
Maximus
0523.DSI Setup and Debugging Guide v1.0.pdf
Checking connection of the flex cable to the LightCrafter Display board is a little difficult for me, unless I disassemble the "Light Engine"....
But I had measured the voltages on the test points after turning the switch to ON : VBIAS is 4.50V. VRST…