Part Number: DM3730 Hi Ti support
Out production is designed with DM3730, used two MMC channel, there are:
MMC1---EMMC
MMC3---SD-Card
And the device bootloader is u-boot-2011.06
Now, the MMC1 can be detected and could read/write EMMC device successful…
Part Number: DM3730 Other Parts Discussed in Thread: TPS65930 , Dear Ti teams:
I am using Flash tools to burn MLO, but he USB seems cann't be recongnize by computer, (hardware is TPS65930 + DM3730 + Micron PoP ddr )
the USB port can recognize…
Part Number: DM3730 Hello support team members,
I am referring to "AM/DM37x Multimedia Device Silicon Revision 1.x Version R Technical Reference Manual".
"26.4.7.4.2 SLC NAND Read Sector Procedure" has the following description.
…
Part Number: DM3730 Dear Ti teams,:
I found a doc is lost connection, could you provide me with a avaiable one, thanks
processors.wiki.ti.com/.../AM37x_CUS_Routing_Guidelines
links: Gone (ti.com)
Part Number: DM3730 Our customer is experiencing a problem with their product that does not start. (DM3730 startup error).
They think that the cause is that the data inside the NAND memory (Micron MT29F2G16A) that stores the program has become garbled…
Part Number: DM3730
I am using omap3730 based SOM and using 5.10.168 kernel.
when running test camera application with histogram enabled, crash is observed(Logs attached- crash_logs.txt). Below are the findings.
1.when dma channel (dma0chan29) is started…
Part Number: DM3730 Other Parts Discussed in Thread: TPS65930 Ti team:
is there any help link to use the Ti Flash tools, for this link is not effective , http://processors.wiki.ti.com/index.php/Flash_v1.6_User_Guide,
Belowing is the flash tools…
Hi Madhurya,
I just tried setting up Ubuntu 10.04, the LINUXDVSDK-DM37X SDK from https://www.ti.com/tool/LINUXDVSDK-DM37X#downloads , and then was able to build both X-Loader and U-Boot from sources without any real problem. Here's what I did:
Downloaded…
Other Parts Discussed in Thread: DM3730 , AM3517 Hi Nick,
There is one another question need your support: Our customer booted Uboot up in DM3730 from SDCard, but their requirement is needed boot from NOR flash,
And some reply has mentioned that should…
Part Number: DM3730 I am developing a touchscreen based GUI application with bitmaps and other graphical elements like graphs, shapes etc on a custom board with OMAP3 AM/DM3730. My application is using open source LVGL library to draw graphic elements…