Part Number: DP159RSBEVM Hello,
I have read in other forum posts that the TUSB3410 eval board needs a different firmware build in order to interface with the EyeScan software (for use with a DP159 chip). How can I obtain this firmware?
Part Number: DP159RSBEVM Other Parts Discussed in Thread: TDP142 , SN65DP141 Hi Team,
Our customer bought DP159RSBEVM but it is not working as shown in the screenshot below. According to our customer,
I am working with the DP159RSBEVM and I followed…
Part Number: DP159RSBEVM Other Parts Discussed in Thread: TMDS181 , TMDS181RGZEVM Dear,
our client use DP159RSBEVM to test and verfy, and we find cannot show pictue. could double confirm what`s something wrong?
as below chart rework EVM block diagram…
Part Number: DP159RSBEVM Tool/software: Code Composer Studio Dear,
We make sure DP Source was can support 4K@60Hz , but connect DP159RSBEVM and we find HDIM signal only can support 4K@30Hz
How to setting EVM? or this is IC limite condiction, like…
Part Number: DP159RSBEVM My customer is evaluating our DP159RSBEVM. Could you please kindly advice the purpose of R1-4 and R6-9 ? If customer use source side == HDMI, How to handle this section? I guess Page#6 show it but I am not sure detail. Thanks…
Part Number: DP159RSBEVM Other Parts Discussed in Thread: TMDS181
Two issues:
1.There are some mistakes in the user´s guide of the Evaluation Module DP159RSBEVM:
sllu224a
a) In the schematics page 4 is double and page 6 (with the reset button…
Hi Kay,
The DP159RSBEVM has a DP input and a HDMI output populated, how are you testing with a HDMI 2.0 input?
Is the source able to see a HDMI 2.0 resolution option? This will depend on the DP++ driver of the source.
If the source is outputting…
Part Number: DP159RSBEVM hi,
I am using the Xilinx Display port(RX) IP v7.0 in my design with Xilinx K7。DP159 as the retimer。When in TP1 Interrupt Handler , the GTX can not locked the recovered clk。Measure the frequency of the AUX_SRCp/n pin with an…