Part Number: DP83561-SP Tool/software: Hi Team,
I am investigating the DP83561, and I noticed there is no max slew rate for the power supplies specified within the datasheet.
Is there a max voltage differential and see if there is any slew rate spec not…
Part Number: DP83561-SP Tool/software:
Hello, in figure 6-1 of the DP83561-SP datasheet, for the power up timing, is T1 with respect to the VDD rail coming up or with respect to clock edge?
We were not certain given the parameter description for T1…
Part Number: DP83561-SP Tool/software: To whom It May Concern,
Hope you're well.
Please allow me to submit inquiry regarding Static Burn-In for device below?
P/N:5962F2021601VXC
Date Code: 2113B
Per SMD, it says "Static Burn-In test shall be performed…
Part Number: DP83561-SP Hi there,
I have a question about the 3-supply power-up for the DP83561. The datasheet shows the preferred method is to power up all supplies at the same time, however, in our case, the +1.1V supply is the first to ramp up, and…
Part Number: DP83561-SP Hello,
I downloaded the IBIS model for this device DP83561-SP from TI website. I used HyperLynx for simulation. I can see variety of drive-strength for 1.8V, 2.5V, and 3.3V rails; however, I cannot find how to change/program these…
Part Number: DP83561-SP
25MHz clock is present on the input pin 26 and also repeated on the CLK_OUT pin 52. All of the power supplies are present. The part is out of reset. No copper link is present. The part should put out 2.5MHz on this pin but it…
Part Number: DP83561-SP Per the TI document SBOA141A that outlines the test flow for QML Class V devices ( https://www.ti.com/lit/an/sboa141a/sboa141a.pdf ), there are Group D tests for Mechanical Shock and Vibration. Can you confirm that the 5962F2021601VXC…