Part Number: DP83620 Hello
We are trying to configure DP83620 tor EtherCAT Network and one of the requirements is to enable FAST LINK LOSS detection.
DP83620 documentation stated fast link loss can be enabled by setting SD_TIME control in the SD_CNFG…
Part Number: DP83620
Hi Team,
Good day! I'm posting this in behalf of our cusotmer as shown below.
Our company bought dp83620 PHY driver from mouser recently. Need driver code support for this. I searched in your website under support, it shows LINUX…
Hi Sreenivasa-san,
We have not been able to determine the cause of the problem, but since the problem occurred in 1 out of 600 units, we will continue to monitor the situation.
This post is closed, and I will post again when the problem occurs.
Thank…
Part Number: DP83620 Hi team
I need the overshoot and undershoot values for DP83620SQ/NOPB 's clock connected at X1 pin
also can you give me the VIH (max) and VIL(min)??
Best regards, William
Hi Sreenivasa,
Thanks for your reply..
We are working on AC701 ARTIX 7 FPGA , So here inside this SOC we have one Microblaze soft processor. Already its having another RGMII hardware connected to this AC701 Eval. board.
I added DP83620 MII interface in…
Part Number: DP83620-EVK Other Parts Discussed in Thread: DP83620 , , USB-2-MDIO Hi,
We just bought the DP83620-EVK evaluation board in order to test DP83620.
We need to acces the MDIO link with the USB port as it is indicated on board user manual.
But…
Part Number: DP83620 Hi Team
We are using DP83620 in our design for MII interface. We could able to meet the trace length of 6inches for MII with zero margin.
Can we able to meet the timings for all the transactions? What is the turn around time of…
Part Number: DP83620 Hi Team,
The IBIS model for the part number DP83620 does not have any IO models assigned for pins RD+/- and TD+/- pins.
Kindly send me the updated model with IO buffer models assigned for SI simulations.
Currently available IBIS…