Part Number: DP83822H Other Parts Discussed in Thread: DP83869 hi team:
my customer is sourcing one device which satisfy with 100BASE-TX and have SGMII interface. do you have the suitable one?
Part Number: DP83822IF Other Parts Discussed in Thread: DP83822H , DP83822HF , DP83822I Hi
My customer XINJE use DP83822IRHBR in PLC , due to supply issue, they need to find other options.
The option as below:
DP83822IFRHBR DP83822HRHBR DP83822HFRHBR
I found…
Part Number: DP83822H Hi team,
Just to be clear, the total load capacitance = C1*C2/(C1+C2) + Cstray? If C1 = 12pF & C2 = 12pF, the total load cap = 6pF + Cstray ==> correct?
For 25-MHz Crystal, datasheet specifies load capacitance between 10pF…
Part Number: DP83822H Hi expert,
My customer plans to use F28388D on a new high power PCS.
They want to use Ethernet to achieve parallel two or more PCS modules.
I want to know whether we can provide a solution which and support functional isolation and…
Part Number: DP83822H Hello,
We have implemented a design with DP83822HF in which we use transformerless (capacitive) coupling in the Ethernet lines (see https://www.ti.com/lit/an/snla088a/snla088a.pdf ). We do it by configuring the output modulation to…
Part Number: DP83822H Hi
I'm in need of a high temperature RJ45 to use with the DP83822H. Anyone know of a connector rated for 125degC ambient temperature?
Thanks in advance
B/R
Jon Eirik S.
TI Oslo