Part Number: DP83822H Hi,
my customer has the following question regarding the linking of the DP83822H:
Within the scope of the EtherNet/IP certification it is necessary that the link can be firmly configured. As a minimum, the device must support autonegotiation…
Part Number: DP83822H In our design we have selected "DP83822H" part. Due to material transit delay ,we haven't received the material. We have a stock of DP83822HF material in our LOM. Please confirm, shall we use DP83822HF material in place of DP83822H…
Part Number: DP83822H Hi,
I need help understanding about the following label on Date Code being noticeably 12 work weeks from each other even though they are under one Lot Code. It appears that there is 2109 under section [D] and also 2121 under section…
Part Number: DP83822H Hi
1. on the EVM schematics, the terminations are connected to 3.3V, as well ass the center tap. how current is sourced to the tap in this kind of connection.
2. why this frvice uses CML IF? if I am right, most Ethernet copper devices…
Part Number: DP83822H Hi Team,
In RMII master mode, RX_D3 is used as 50MHz clock output by default. While, RX_D3 can also be used as strap pin, and in datasheet, we see the example of pull-up or pull-down (Mode1/4) design recommendation. How can we strap…
Part Number: DP83822H Hi Geet,
My customer has the problem to pass IEC61000-4-2 immunity test when he activates BIT 3 RX Error BIT0-2 == 0. If they activate BIT 2 , so MLT3 criterion they pass the test. The customer uses a ESD Gun. We first tried to improve…
Part Number: DP83822H Hello,
With reference to below part number,
TI : DP83822
We are using this phy with HI3516AV300 and many other soc.
Does MDC of DP83822 have an internal Pull Down inside? If yes, What is Pull Down value.
We could not find such …