Part Number: DP83825EVM Hello,
I am interfacing a DP83825 Ethernet PHY evaluation board with an i.MX RT1042 MCU.
The i.MX RT1040 EVK originally uses a KSZ8081 PHY . I removed the KSZ8081 and its related jumpers, then connected the RMII signals (TXD…
Part Number: DP83825EVM Hi Team,
customer test EVM and found the LED0 is off while powered on.
When connecting EVM with the laptop and running GUI to detect the ID, there is an error message popup.
Please help.
Thanks.
Part Number: DP83825EVM Tool/software: We want to EMI simulation in PCB with DP83825(Ethernet IC).
So do you have a IBIS Model, DP83825 or not, could I receive another simulation source model at DP83825 for EMI simulation?
Part Number: DP83825EVM Tool/software: Hi Team,
I want to use DP83825 PHY in the project. want to know about IEEE 1588 Time stamping, is the IEEE 1588 Time stamping supported?
The PHY is categories as copper, so is fiber not supported and what is…
Part Number: DP83825EVM hi, team
Is the schematic (snlr041a) of DP83825EVM consistent with the actual DP83825EVM evaluation board?
From the schematic, it shows only two pins of MSP430(pin 46 and pin 47) are connected with DP83825. it is right?
Part Number: DP83825EVM Tool/software: Hi,
We are currently using the DP83825 in our design and have started the proof of concept. I can read and write PHY registers through the STM32H573I-DK, but I am unable to read data in the STM32 MAC. The link…
Part Number: DP83825EVM
Tool/software:
Hi,
I want to interface the DP83825IRMQR to STM32H573I. please help us with the required drivers and utilities. we are using Keil IDE and uLink debugger.
Regards,
Harsha
Part Number: DP83825EVM
Tool/software:
Hi,
I wanted to interface DP83825IRMQR to MCU with RMII interface, so for the RMII REF Clock do I need to connect 50MHzOut/LED2 to the REF_CLOCK pin of the MCU or Need to connect directly from the Crystal Oscillator…
Part Number: DP83825EVM Tool/software: Hello,
Does LED0/S (ANEG _Dis) Pin 4 and LED2 Pin 2 can be configured for Link/Activity and Link Speed indications and shall be configurable for different functions.
Regards,
Harsha
Part Number: DP83825EVM Other Parts Discussed in Thread: USB-2-MDIO I am trying to use a pair of DP83825EVM boards to add two 10baseT interfaces to an FPGA evaluation board. I have added zero-ohm resistors in the pads connecting RMII to J9 and connected…