Part Number: DP83849I Other Parts Discussed in Thread: DP83869 Tool/software: Hi,
I need help in finding a network cable tester/diagnostic IC that can acheive the following tests:
- Wire Map Test - Checks for proper pin configurations and identifies…
Part Number: DP83849I Other Parts Discussed in Thread: MSP430F5529 , Hello experts!
Could you please tell the procedure to monitor all the register values in dp83849ifvs IC with the help of msp430f5529..
i know only few registers but i would like…
Part Number: DP83849I Hi team :
my customer is sourcing dual RMII phy, so i think the DP83849I is good to use.
when we check the spec , there are some question we confused:
1/ Can both RMII be configured as RMII master mode?
2/ The value of the…
Part Number: DP83849I
Hello, greetings from Istanbul Pin No. 4 PHYAD1 (RXD0_A) and Pin No.5 PHYAD2 (RXD1_A) both shared Strap PHY Address select option and RMII Mode receive data signals, RXD[1:0] at MAC-A Port By default These pins are PD. And i would…
Part Number: DP83849I Hi expert,
We want to use one channel of 83849 to receive data, and then send the received data through another channel. I think that specification 5.4.4.3 should be able to realize this function, but there seems have request on…
Part Number: DP83849I Other Parts Discussed in Thread: DP83848C , Hi,
I'm using DP83849IVSX/NOPB part in my design.
The Ethernet switch (SJA1105QELY) and Processor (i.mX6solo) is interfaced for MII (Media-independent interface) for LAN.
The SJA1105P…
Part Number: DP83849I Hello team,
I received a question from the customer.
Is the only way to stop the output of the SLP signal, etc., by controlling the RESET signal?
The customer's situation is as follows, During normal use, the device is operated…
Part Number: DP83849I Dear team,
My customer want to use DP83849IF to replace DP83849I because of supply shortage.
1. Do you have any suggestion about what they need to pay attention to? Will it be a smooth transfer?
2. If they don't need the flex…
Part Number: DP83849I Other Parts Discussed in Thread: TM4C129ENCPDT , , DP83869HM My application is building off of a previous design using a copper ethernet port into the built-in 100BASE-TX MAC/PHY in the TM4C129ENCPDT micro. My directive is to convert…