Part Number: DP83867ERGZ-S-EVM Hi,
I would like to report an issue observed with the following setup:
First laptop connected to a first DP83867ERGZ-S-EVM board via RJ45
First DP83867ERGZ-S-EVM board connected to a second DP83867ERGZ-S-EVM board…
Part Number: DP83867ERGZ-S-EVM Dear TI Support Team,
I am working with a DP83867ERGZ-S-EVM evaluation board and need assistance enabling test pattern transmission for gigabit Ethernet signal integrity measurements.
My Setup:
EVM: DP83867ERGZ-S…
Part Number: DP83867ERGZ-S-EVM
I’ve got the tool running and I can access the registers. However, the changes are not being saved, and after a reboot the board always comes up again in the default 1000Base mode.
How the configuration can be stored…
Part Number: DP83867ERGZ-S-EVM Hi, I'm using the DP83867 SGMII dev board to evaluate replacing using this part to replace a 1G copper SFP module with an FPGA.
Does the PHY have to be setup over the MDIO interface before it will work in SGMII mode? I…
Part Number: DP83867ERGZ-S-EVM Other Parts Discussed in Thread: DP83869 , DP83867CS Hello TI Support Team,I’m working with the DP83867ERGZ PHY connected to an NXP SJA1110 Ethernet switch through an SGMII (4-wire) interface. The MDIO of the PHY is also…
Part Number: DP83867ERGZ-S-EVM I want to see how the signal looks like on the Oscilloscope with a Diff probe for Clock and Data. I have two boards? Do I need an direkt Link with both? Do I need to change the Jumper? How can I have a communication?
Part Number: DP83867ERGZ-S-EVM
Tool/software:
Hello,
I openend this case some weeks ago, but unfortunately I could not make the measurement in time and case was closed after some days.
The original case was DP83867ERGZ-S-EVM: RFSoC (Ultrascale…
Part Number: DP83867ERGZ-S-EVM Other Parts Discussed in Thread: DP83867E , Tool/software: Need a dwg or stp file of board DP83867E SGMII EVM to know dimensions