Part Number: DP83869HM Other Parts Discussed in Thread: DP83869 Hello,
I've read the other E2E forumn posts on this topic. I want to know if there were any die changes between the EM pre-production and HM production variants of the DP83869 device or…
Part Number: DP83869HM Dear Technical Support Team,
I would like to use the DP83869HM in a Two-Supply Configuration.
Figure 9-9 in the datasheet shows the power-on sequence, but there is no diagram for the power-off sequence.
1) Are there no specific…
Part Number: DP83869HM Hi,
I would like to know if it possible to invert the +ve and -ve of the SGMII pair on the DP83869HM? Specifically just the RX/SI pair (PIN 16 and 17).
I require this to make PCB layout more simple.
I am using the device in…
Part Number: DP83869HM Hello, Unfortunately I was not able to respond on my previous question: https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1639651/dp83869hm-dp83869hm-no-link-detection-in-1000base-t-configuration?tisearch=e2e…
Part Number: DP83869HM Other Parts Discussed in Thread: DP83869
Hi Team,
I am using the DP83869 PHY with the J0011D01BNL RJ45 connector in my design.
Is it recommended to use 49.9E pull-up resistors to 3.3V at the PHY-to-RJ45 interface for this…
Part Number: DP83869HM Other Parts Discussed in Thread: AM6442 , DP83869 Hello TI Team,
We have a custom board based on the AM6442 with a DP83869HMRGZT connected to an SFP cage. We would like to determine whether our current hardware design can support…
Part Number: DP83869HM Other Parts Discussed in Thread: DP83869
DP83869HM in RGMII-to-SGMII bridge mode:
During SGMII auto-negotiation, are the configuration/control words
transmitted as standard /C/ ordered sets per SGMII spec,
or are they…
Part Number: DP83869HM Other Parts Discussed in Thread: DP83869 , DP83869EVM Hi,
We are using DP83869HM in our design
1)Using DP83869 along with STM32MP257D Processor in RGMII to copper mode,firstly Link got established in 10/100/1000MBPS from…
Part Number: DP83869HM Other Parts Discussed in Thread: DP83869 Hello,
Background:
We have a custom board with a DP83869HM PHY connected to an FPGA acting as a MAC over 4 wire SGMII interface. The PHY is configured to SGMII-to-Copper Ethernet Mode…
Part Number: DP83869HM Other Parts Discussed in Thread: DP83869 Hello,
I have a custom board with a DP83869 :
Connected with RGMII + MDC to the application processor
I am able to read/write all MDIO registers (std + extended set) from the linux…