Part Number: DP83TC811R-Q1 Other Parts Discussed in Thread: DP83TC811 Hello Expert,
The customer did high temperature testing for DP83TC811R-Q1 and there was a link-down issue happen. After checking the register value, only 0x0017 becomes different…
Hi Carlos,
The 10BASE-T1L products are generally suitable for 2000+ meters. The 100BASE-T1 products have been tested with cable lengths up to 15 meters. The 1000BASE-T1 products are also generally intended for cable lengths of 15 meters or less but…
Part Number: DP83TC811R-Q1 PHY receive data issue
after systems start up, can not see any data received from DP83TC811R-Q1 transceiver
PHY is link up, SQI = 75,
during running time, we log the some registers value for your reference (all is hex…
Part Number: DP83TC811R-Q1 We currently use DP83TC811RWRNDTQ1 chip as the PHY chip of the BroadR-Reach interface of our imaging radar, and the test found that the output data of the BroadR-Reach interface stops abnormally under the condition of long-term…
Part Number: DP83TC811R-Q1 Hello,
we are using the DP83TC811R-Q1 Low Power Automotive PHY. The Phy has the automatic function to change the polarity if the wires are not correctly connected. We want to know when this happens, which parameter does describe…
Part Number: DP83TC811R-Q1 Hi Experts,
My question is that how to configurate the DP83TC811R-Q1 in below situation?
1. Under uboot, does the phy chip register require special configuration to function properly?
2. The SOC currently communicates…
Part Number: DP83TC811R-Q1 Hi Expert,
Could you please help me understand the accuracy of internal temperature sensor for DP83TC811R-Q1?
Thanks!
Ethan Wen
Part Number: DP83TC811R-Q1 When the device is configured, initialized and up and running, in order to set link status to active/down only register 0x485 (PCS_CTRL1) bit 12 should be set/cleared.
1) Is this correct?
2) If this is correct, is such bit…
Part Number: DP83TC811R-Q1 Hi Team,
I would like to know the maximum transmission distance during TI's evaluation.
I found that it transmits 40m when using shielded cable.
Is there a 100m transmission capability for 100Base-T1?
Regards,
…