Part Number: DP83TC812S-Q1 Hello, can you please provide me information about current consumption for DP93TC812S if I am using SGMII interface with the following voltage rails: VDDIO and VDDA are connected to the 3V3 and VDDMAC is connected to 1V8. All…
Part Number: DP83TC812R-Q1 Tool/software: Dear sir.
Our team has purchased phy chip for dp83tc812 from ti, but I have some problems when I am using the driver file for dp83tc812 under linux written by you. The details are as follows
We are under linux…
Part Number: DP83TC812S-Q1 Tool/software: Hi team.
Our customer found the err about the datasheet.
On the 8.3.1.2 Electrostatic Discharge Sensing 0X310 [6] 0 = cable OPEN ; 1 = cable Short
But on the 8.6.2.39 TDR_TC1 Register (Address = 310h) [Reset …
Part Number: DP83TC812S-Q1
Tool/software:
HI,
PHY can Link UP,PHY can output 25MHz clk. but it cannot ping.
Is it possible to loop back?
How can I confirm that MAC to PHY can communicate?
The PHY driver is downloaded from here.
www.ti.com/.../DP83TC812S…
Part Number: DP83TC812S-Q1 Tool/software: Hello, we need to adapt the Ethernet and power amplifier driver on the AG35 module, I wonder if you can provide the driver source code? thanks
Ethernet chip model: DP83TC812S
Ethernet chip communication: RGM…
Hi Norio,
Norio Hasegawa said: (1) Did you find anything out of the materials?
Other users have also encountered 100BAE SGMII NG, so I don't think it's a problem with the circuit or pattern.
Is there any way to investigate the problem? Can you…
Part Number: DP83TC812S-Q1 Other Parts Discussed in Thread: DP83TG720S-Q1
Hi,
Can TI provide us with the driver for the DP83TC812S? Our SDK version is ti-processor-sdk-linux-adas-j784s4-evm-09_00_01_03
Thanks!
Part Number: DP83TC812S-Q1 Hi team,
SNLA389A shows that the PMA test mode register is 0X0836.
But the register given in the datasheet is 0X1836.
Which one is correct? How should we choose the configuration?
Thanks
Xiaoxiang
Part Number: DP83TC812S-Q1 Hi,
Could you explain at what condition the device will transmit the WUP and WUR?
Let's discuss the condition at which two DP83TC812 connect together, for convenience.
I think the device will transmit a WUP after local…
Part Number: DP83TC812S-Q1 Hi, TI
We're experiencing a link down issue.
Register 0x871 shows that the current SQI value is 0, register 0x1 shows that the current state is Link up, and it is currently not able to communicate with the peer.
After…