Hi Stan,
We tried to desoldering R0664,R0619 and pull the CE pin to high by 10K resistor,but not improve.
From the SCH,have you find some hardware problem?Could you help check our DRA725 SCH?
Part Number: DRA725 Tool/software: Linux Hi,
We used DRA725 as our Automotive processor ,but we met some problem with CAN module.
1. can0 schematic diagram
cpu
TJA1042T:
2.software config with can0 reuse
3.the development…
Hi Lin,
This error [ 63.294201] omapdrm omapdrm.0: could not remap: -12 (3) shows that, system is running out of TILER memory. There is exactly 128MB of TILER memory available and graphics buffers are allocated from TILER memory.
On kernel 4.4 based…
Part Number: DRA725 Hi ,
I have Desay 187B Stereo model in my Car and it has navigation issue, most of time navigation arrow doesn't follow me. It start well but after some it loses direction.
In this design "DRA725LGABCRQ1" is used, which is infotainment…
Part Number: DRA725 Tool/software: Linux Hi TIs:
Due to some reasons, we need to do an experiment which set the frequency of MPU to run at 800 MHz
According to the spec, the OPP_NOM of DRA725 is 1000 MHz
Is it possible to set MPU frequency lower…
Part Number: DRA725 Hi all,
Would you please helping to check the reflow times about those items for my customer's reference? Thanks.
DRA725AMGABCRQ1
DRA755BMGABCRQ1
DRA751BMGABCRQ1
Best regards,
Gary Teng
Hi Anand,
TEST case 4 run failure, second loop break for error msg:
failed to create egl surface
source code:
init_gbm();
while (1) {
init_gl();
exit_gl();
}
exit_gbm();
Regards,
Ya Lin
Suggested answer from e2e similar question:
e2e.ti.com/.../2195262
e2e.ti.com/.../2486764
eMMCv5 part would be backward compatible with V4.5 hence you would be able to use a V5 part on DRA7x device.
The features from V5 spec will not be available…