Part Number: DRA725 Tool/software: Linux Hi,
I rebuild ipumm follow:
make ducatibin:
I install the ccsv6 tool which option:
how to option.
Regards,
Cesar.
Part Number: DRA72 Other Parts Discussed in Thread: DS90UB933-Q1 , DS90UB936-Q1 , How to connect DRA725 with the serializer DS90UB933-Q1? The Deserializer is DS90UB936-Q1 .
Hi Kevin,
The patch will not work on 7.03 GLSDK release.
The MMC framework/driver has changed a lot between 7.03 and 3.04. The patch also has a dependency on Thermal framework which also has changed between the two. It's better to switch to latest version…
Part Number: DRA725 Other Parts Discussed in Thread: AB15 Tool/software: Linux Hi,
now i use the battery to power the RTC module;
i add the driver that omap-rtc to kernel and i can measure the RTC_OSC_XI_CLKIN32 is 32.768KHz;
but i set date and…
Part Number: DRA725 Tool/software: Linux Hi,
sdk: ti-processor-sdk-linux-automotive-dra7xx-evm-03_02_00_03
i don't know what are they doing that ipc_ipu ipc_mpu ipumm.
can you explain?
thanks,
Cesar.
Part Number: DRA725 Tool/software: Linux Hi Expert,
DRA7xx TRM say it supports NV21 format input, so far the Linux DRM/DSS driver can not input the format as NV21. Would you please suggest how to change the driver code to support that? If need reprogram…
Hi Ya Lin,
IVAHD control will need to be done via either of the IPU, you can still use this for your private purpose, however you would need to integrate the IPUMM into one of the IPU for controlling the IVAHD.
If this doesn't answer your question…
Part Number: DRA725 Tool/software: Linux Hi,
examle: videnc2test.c
encoded the h.264, the configue:
I look at the ‘XDM_ENCODE_AU’ configuration instructions:include head
but the h.264 file without head info--PPS,SPS:
or can you offer…
Samgyung,
If you are using DR74x which has two video PLL's , you should not have a problem at all. All the patches I shared were assuming that you were on DRA722 based on the subject of the post "Linux/DRA722: dra722/dra725"
If you look at dra7…