Part Number: DRA726
I tried to follow the instructions on
U-Boot 2019.01
Please apply this patch http://processors.wiki.ti.com/index.php/File:0001-u-boot-configs-Enable-configs-for-Early-boot-support.zip on U-boot repository in board-support to enable…
Part Number: DRA726 Other Parts Discussed in Thread: DS90UH925Q-Q1 , DS90UH926Q-Q1 , DS90UB949-Q1 , DS90UB948-Q1 As I am working on getting our analog camera working with the VIsion SDK I noticed that it has support for DS90UH925Q-Q1 and DS90UH926Q-Q1 Is there…
Part Number: DRA726 Hi,expert,
My customer has a requirement, They use the fb0 to display when upgrading the system.
In our VISION-SDK, I have checked /dev/fb0 node, It's not exist. I have checked the kernel. and enable the DISPLAY_ON_A15_LINUX. Also…
Part Number: DRA726 I am working from home because of the Coronavirus, so I am using my home login instead of the one I use at ACTIA Corp.
That way I can see messages on my Mac. I cannot access the ACTIA Web mail from Safari.
I have created a yocto build…
Part Number: DRA726 Tool/software: TI C/C++ Compiler I am teaching a new programmer about yocto and a yocto tree that we've use for a product that we are shipping doesn't compile.
I have not changed anything in it.
It is based on SDK automotive…
Part Number: DRA726 I get some strange errors on git.ti.com
Example :
git clone -b ti-linux-4.19.y git://git.ti.com/ti-linux-kernel/ti-linux-kernel.git linux-4.19-ti Cloning into 'linux-4.19-orig'... fatal: unable to connect to git.ti.com: git…
Part Number: DRA726 We have a customer who asked if I could get their application to start within 5 secs.
I have a problem with that because it takes about 17 secs to get to weston and then weston takes about 5 seconds to load the application.
Is is…
Hi Michel,
Thanks for the update and glad to hear that the weston is booting now.
The logs seem to be ok, were you able run any of the example weston clients - eg. weston-flower etc.
Some comments on the logs
Unable to use first choice EGL config with…
Part Number: DRA726 Hi Team,
I want to test the sound card in vision-sdk, But can't find the soundcards. Log as below: Can you help to check ?
$ aplay -l
aplay: device_list:268: no soundcards found...
$
root@dra7xx-evm:~# lsmod
Module …
Part Number: DRA726 Hi,
We are in the SW architecture design phase for an Android O 8.1 based IVI + RVC custom product for one of our customers.
SoC under consideration is DRA72x.
My query is,
Is there an OTA upgrade reference implementation available…