Part Number: DRA744 We have a hardware platform which utilizes Jacinto 6 SoC as its main application processor. Its OS is Android . The achieved performance on it is not satisfactory. We are working to find out whether we might discover a way to enhance…
Part Number: DRA744 Tool/software: TI C/C++ Compiler The wiki article mentions that for IP-Protection 'hide' and 'unhide' could be used to remove symbols from e.g. a codec library. That's exactly what one of my customers is trying to accomplish. How…
Part Number: DRA744 Other Parts Discussed in Thread: DRA742 Tool/software: Linux Hi Community Members,
I am using latest SDK ti-processor-sdk-linux-automotive-dra7xx-evm-03.03.00.03 for Vayu EVM Rev H Board.
I need to configure MCASP1. But I am not able…
Part Number: DRA744 Other Parts Discussed in Thread: TUSB1210 Tool/software: Linux Hi,
I'm using DRA74x chip and Linux version 3.14.57,I am here to configure the TUSB1210 chip, it can work normally, but the USB1 port into the mouse system will hang dead…
Part Number: DRA744 Hi Everybody ,
please on DRA74x ( and future eveolution pin2pin ) I would like to use eMMC as boot .
now I see on TRM , MMC1 ( the one I use ) is for SDcard boot : do you see any issue in using eMMC ?
anything to cross check to make…
Hi,
Can you confirm e52241 is accessible via I2C, and the required configuration is set properly in the registers? E.g. 2MHz, 500mA, etc in the Setup_SMPS register?
Regards,
Stan
Part Number: DRA744 Hi,
Facing VIP Video pipeline freeze at higher system load. Made sure there is no issue with camera signal, driver capture path and application frame handling.
While the sytem load or L3 data traffic is high, the VIP HW pipeline froze…
Part Number: DRA744 Hi ,
This is customer board , TP IRQ ( GPIO6_11 ) triggered level is set to "IRQ_TYPE_LEVEL_LOW" , it couldn't be triggered in normal after android boot completed .
But the IRQ can be triggered at follow operations :
1. After…
Part Number: DRA744 Other Parts Discussed in Thread: TVP5158 , SYSCONFIG Hi ,
This is customer board , We use ADV7180 as CVBS decoder ,which output the interlaced video .But we found that there are some unexpected horizontal stripe on the screen .
We have dump…
Hi Subhajit,
yes, kmscube always works.
After another bit of debugging, the issue seems more linked to lack of memory for applications, rather than for graphic stack (we can observe the kernel killing application because of out of memory errors).
Regards…