Part Number: DRA744 Tool/software: Linux Hi TI,
I'm using TI J6 platform(Android, 6AM.1.3), we make a camera adapter to connect YUV camera to "VIN[1]A".
Sensor output: 1280x800(30fps, YUV422-8bit), hardware interface: VIN[1]A_D[0-7],VIN[1…
Part Number: DRA744 Hi
I am doing USB 3.0 compliance test that in the test need to get some pattern LFPS, CP0 and CP1 by USB of DRA744.
I can get LFPS pattern when the USB port attach to the scope and it can pass the LFPS test as below.
For next step…
Part Number: DRA744 Other Parts Discussed in Thread: TDA2 Tool/software: Linux
Hi ,
I use the RGMII interface connect with Marvell Ethernet SW (88E6390).
I set RGMII delay setting enable ( rgmii-id ) but it seems not work.
Below is…
Part Number: DRA744 Tool/software: Linux Hi,
I am seeing an error when performing playback with an Android app on my device. The error log is below: E/OMX_VIDDEC_COMMON( 4725): E/OMX_VIDDEC_COMMON( 4725): Process function returned an Error... E/OMX_VIDDEC_COMMON…
Part Number: DRA744 What does the 'D' in "DCAN" represent? (DCAN => Controller Area Network)
"The Controller Area Network (CAN) is a serial communications protocol which efficiently supports distributed real-time applications....…
Part Number: DRA744 Tool/software: Linux
Good morning,
I'm working on board with DRA7xx, 4 videocamera inputs, using VIP and VPE on Android JB system, Linux kernel 3.14; the VPDMA is loaded with the FW "vpdma-1b8.fw".
Every (average)…
Hi Angela,
Thanks for your response, Sorry I wasn't able to respond earlier. The previous issue is no longer an issue. However, I see a new error with a different app. The error log is below:
E/OMX_VIDDEC_COMMON( 4725):
E/OMX_VIDDEC_COMMON( 4725…
Part Number: DRA744 Tool/software: Linux Hi,
I have booting the DRA744 on uboot process.
Some time will stop the boot process that I have check the power sequence and power of PMIC is ok.
The related log as below,
Could any one please tell me how can…
Part Number: DRA744 Tool/software: Code Composer Studio I'm facing an issue with the TI DSS debug scripting. My code is C++ based, using the TI simulator, and I am trying to set a breakpoint on an ASM label inside a class function, and: - Read a local…
Part Number: DRA744 A customer is asking a general question and I am repeating there for the E2E community:
Can a Silicon Pad be added to the top-side of a Jacinto 6 (DRA74x) device for heat sinking?
Doing so might apply excessive pressure to the Jacinto…