Part Number: DRA745 Hello, TI teams:
I am using the DRA745 (android 8.1 kernel: Linux 4.4.117)chip for development. I set the machine to mtp mode and connect to the PC. The I copy some files into the machine. But only small file which is smaller than…
Hi David,
Yes we are using ipu2 core, and dra74-ipu2-fw.xem4 is generated with IPUMM_INCLUDE=yes
using https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/791/flash_5F00_scripts.tar.gz
The isssue is not reproduced.
Thanks…
HI David ,
Thank you for all your support ,
Sorry for the late , the last time i compared my .config files with yours , and found them a little bit similar , also the reproducing of the issue is decreased but it can happen so we decide to change the…
Hi Yordan
Your solution for my case, look like emif1 config as 16bit and emif2 also config as 16bit.
This solution look fine ! Thank you!
Further question.
May I config emif1 as 32bit and disabled emif2 ?
Part Number: DRA745 Hello,
A customer is reworking omap_hsmmc driver (from 6AL1.2 release based on kernel 3.14) for AUTO_CMD23 support. They have previously successfully hard coded this support by setting MMC_CAP_CMD23 in mmc->caps in hsmmc_probe()…
Hi Chokri, If I understand correctly, you are using DRA745 EVM and instead of LCD panel you are using HDMI display and RVC output is shown on HDMI screen. Correct? Regards, Vishal
Hi,
Its been long since any update on this thread.
I hope the issue is resolved.
If not then please reply below or create a new thread for different issue.
Regards,
Anuj
Hi,
I haven't heard back from you, I'm assuming you were able to resolve your issue.
If not, just post a reply below (or create a new thread if the thread has locked due to time-out).
Regards,
Yordan
Hi,
Tiler memory is a must for IVAHD because it's designed like that & you can use the CMA pool for the rest of HW IP like VPE, GPU, etc.
Thanks
Gaviraju