Part Number: DRA74P Tool/software: Hi Team, here is Jitendra.
we require 32bit Microprocessor having 3 ethernet ports each 1Gbps, 1 CAN2.0B or CAN FD, 7 UART, these are primary features. please don't suggest DRA, AM & TDA series below link, i already…
Part Number: DRA74P
Our customer returned to us a board where sometime, after the DDR setup, DDR controller and DDR3 are not able to go up and running.
On board we have jacinto+ DRA746PPIGABZRQ1 and 4 x MT41K512M16VRP-107AATP memory (2 x each…
Part Number: DRA74P Hello,
We are using the DRA7x with Linux BSP w. kernel 5_10.
I understand that normally ethernet frames can be routed to specific queues using VLAN priority values.
Still, in our use case, all packets have their VLAN tags removed…
Part Number: DRA74P Other Parts Discussed in Thread: DRA742 , TPS25830A-Q1
Current we are doing board bring up activities of our product (DRA742) and need support in flashing the DRA742.
USB3.0 connected is to USB1 port of DRA742;but when tried…
Part Number: DRA74P Other Parts Discussed in Thread: DRA742 we are using Wifi module connected to J6 DRA742 on PCIe interface. We are unable to detect the Wifi even when all necessary signals are provided
Part Number: DRA74P Hi,
The IBIS model received for DRA74x series has issue with HDMI output Buffer Model.
The voltage received at receiver pin is in nano or micro volts. Even with a 100 Ohm termination the voltage levels are not better as tested…
Part Number: DRA74P Hello,
It appears STR is not working for this part and this version of the Linux kernel. Yes, it is very old. I found a pull request that claims STR is working for the DRA7.
patchwork.ozlabs.org/.../
It was introduced in 3.18…
Part Number: DRA74P Other Parts Discussed in Thread: DRA746 Goodmornig
We are usign DRA746P chip at 1.5GHz on a board with Android4.3 and kernel3.8 with 2GB of RAM (DDR3).
We have kernel crash when we add module related to Ethernet (our phys are…
Part Number: DRA74P Dear Processor Team,
very quick question, my customer is redesigning a display application moving from J6 to J6P (DRA746P). on top of power supply etc he was asking if the Crystal oscillators need to be reviewed to guarantee matching…
Part Number: DRA74P Hi everybody ,
I m updating the board to have 4GB RAM
I m on Android JB + K3.8 , any suggestion to run a test on DDR without rebooting ?
I need when doing production and runnig ful functional test for example in temperature on…