Part Number: DRA756 Hi
Can we get support for the J6 board. We have a product that we developed based on the J6. Now would like to modify the board for an other project.
In this senerio can we get the support for the same.
Also would like to know…
Part Number: DRA756 Other Parts Discussed in Thread: DRA75 What is the instruction width [bits] for DRA76
Also what are graphic standards, Video Codecs supported by DRA75
Part Number: DRA756 Hi Experts, Good day. Our customer is asking below information.
In one of our designs, we are using DRA75x, DRA74x chip. One of the eMMC interfaces plans to use HS200 (200MHz) SDR mode. I could able to find the setup & hold time…
Part Number: DRA756 Render node /dev/dri/renderD128 fails
Steps to reproduce:
#start weston using desktop shell
export WAYLAND_DISPLAY=/run/wayland0
# Does not work. By default it tries to use the offscreen render node
# /dev/dri/renderD128.…
Part Number: DRA756 We have introduced an error in our code which occasionally stimulates reporting of a 2 bit OCMRAM ECC error in OCMRAM1 shortly after power up. We do initialize and clear out any OCMRAM errors at power up of the OCMRAM module, however…
I don't know the meanings of those errors. Are you running fsck on mounted file system? There is a note in man page of fsck tool saying this is not safe to run fsck on mounted file system. Also, do you unmount file system every time you power off the…
Part Number: DRA756 Hi.
sdk: PROCESSOR_SDK_VISION_03_05_00_00
For the same software, only the SOC of the two boards is different. One uses tda2s and the other uses dra756.
Tda2s can use EMMC ddr50 mode.while dra756 cannot use ddr50 mode,Dra756 can…
Part Number: DRA756 Other Parts Discussed in Thread: STRIKE For the current shipped machine, the customer returned three core boards, and found that CPU the power short circuit, short circuit places have similar places, VDDSHV8 power short circuit, EVM3V3…
Part Number: DRA756 Other Parts Discussed in Thread: TDA2 Hi,
i have been debuging the single camera usecase. hardware structure is that: ar0231 > ap0202 > ds90ub933 > ds90ub934 > tda2(ipu2) > HDMI 1920*1080.
everything goes well but displaying. The…