Part Number: DRA75P Kindly can you provide me with the maximum resolution of " Image Signal Processor " for this part DRA75P?
Appreciate your fast response.
Part Number: DRA75P Hello Support Team,
Can you provide me with the AutoSAR version for MCAL for DRA75P and its availability or release date?
I appreciate your fast response.
Thanks
Ahmed Sabry
Part Number: DRA75P Hello Support Team,
I found in the datasheet that this product supports over 64 logical channels as follows:
So kindly can you provide me with the meaning of Logical Channel?
Thanks
Ahmed Sabry
Hi AClemotte,
It will be good to see the scope shots to determine if the EN of these devices is going low OR if the PG is being tripped on the output voltage/current limit. It is hard to tell what is actually causing this event to happen without visual…
Part Number: DRA75P HI everybody ,
I m using DR746 family and now thinking to use DRA756P or DRA746P .
now I did a compare on the web and got the attached table .
I can see “TI functional safety” field under 746 but not under 75P ( see attached…
Part Number: DRA75P Other Parts Discussed in Thread: DRA744 Hi Everybody ,
I need to move in same PCB from DRA744 to DRA746P or DRA756P -
I m now on DRA744 on Kernel 3.8 , and Android 4.3 : when moving apart form setting operating conditions ( like…
Part Number: DRA75P Other Parts Discussed in Thread: DRA744 Hi everybody ,
I would like to use on a DRA744 board J6+ for higher DDR speed .
questions :
- are they pin2pin compatible ? anything particular to take care ?
- I see J6+ is about 1.3…
Part Number: DRA75P Other Parts Discussed in Thread: TDA2 , TVP5158 Is there an off-the-shelf CSI2 output camera module available for the J6/J6+/TDA2/TDA2+ EVM that mates directly to the CSI2 connector (J8 on J6+ EVM, J5 on J6 EVM)? That is, need a direct…
Part Number: DRA75P
Tool/software:Android->u-boot->recovery
Hi,TI.The board I used is j6evm5777 board,and cpu is dra752-GP.Besides,the code source is 6ao1.1.
I want to enter the recovery mode from the u-boot,and I find that changing the…