Part Number: DRA76P Hello,
We have an issue capturing images with the vip1 and adv7611 in linux. We think the chip is correctly configured for 1920x1080 30Hz but the captured images are not fine, they are cropped, flattered and the color is not ok.…
Part Number: DRA76P Tool/software: TI C/C++ Compiler Hello,
I'm working on customer board based on DRA76P Soc, using SDK version 03.02 for RVC use case.
Now, the RVC is configured to show/hide using GPIO7_18 on EVM board.
I need to use another GPIO…
Part Number: DRA76P I'm using a TO jacinto j6+ board.
I want to use the EVE processor to run Android/ Linux and communicate with dual core A15s running Arago dist of Linux over IPC.
Is this possible? Do you see any issues
Part Number: DRA76P Hi,
Using SDK 3.02 with prebuild android 8.1.1 :
We are trying to boot Android on a custom board based on DRA76P with HDMI display only:
Display OK but color are inverted :
hdmi0: connector@1 { compatible = "hdmi-connector…
Hi Vishal,
Thanks for replied.
There is any guide for testing the fpd display and HDMI on my DRA76P Android device ? if yes can you please share it .
I have share full modetest output log you can find it.
trying to open device 'i915'...failed…
Part Number: DRA76P On trying to run make u-boot in the SDK "ti-processor-sdk-linux-automotive-dra7xx-evm-6.00.00.03". I get the following error:
make -C /home/nalin/ti-processor-sdk-linux-automotive-dra7xx-evm-6.00.00.03/board-support/u-boot CROSS_COMPILE…
Part Number: DRA76P Dear Mr./Mrs,
We are working on a custom board that includes a DRA76P with both QSPI and eMMC flash devices. QSPI P/N is S25FL256ASGMFV001 and eMMC is MTFC8GAMALNA-AAT.
QSPI is working fine. But not the eMMC memory. They are connected…
Part Number: DRA76P Tool/software: Linux I have a Jacinto DRA76P running Linux.
1. I need to bringup Android on this.
2. I need the type 1 hypervisor to run both Android and Linux on it.
Please let me know how I can achieve the above.
Part Number: DRA76P Hi all,
We are observed that simple GUIs don't flow correctly, thinking about this issue, we guess that this problem is related to that we don't use de GPU in the soc.
My questions are, Is it possible? how can we check that?…