Part Number: DRV2511-Q1 Tool/software: Hi Sirs
Question:
1. We input positive voltage PWM signal(0~3V3) to DRV2511 with PVDD 5V => Driver could amplitude normal output from 3V3 to 5V
2. As PVDD 6~18V => Driver will produce impluse waveform instead…
Part Number: DRV2511-Q1 Tool/software: Hello,
I'm having trouble driving an actuator with the DRV2511-Q1. I'm using a function generator to provide an arbitrary waveform to the input, but the measured load current doesn't match the expected output.…
Part Number: DRV2511-Q1 Tool/software: Hi Team,
Could you please kindly review this schematic for DRV2511-Q1? Any comments can improve the design would be appreciated. Thank you!
Best,
Frank
Part Number: DRV2511-Q1 Tool/software:
Noise is present on the PVDD/AVDD Vbatt supply rail, as well as on VCC1—the 3.3V regulator output from the CAN SBC, which is tied to the INTZ pull-up resistor. One chart illustrates Vbatt (orange trace), connected…
Part Number: DRV2511-Q1 Tool/software: Hello, We are having an issue with this driver. With IN+ = 3.3 v, IN- = 0 v, EN = 3.3v, we are getting a fault every 8 seconds. Only thing we do is set the EN to 0 v for 10 ms then reset IN+ = 3.3 v, IN- = 0 v, EN…
Jax Lin said: 1. How to import to Haptic Control console?
What do you want to import? Please clarify
Jax Lin said: 2. Does it have any guideline to apply this FW?
The firmware can be downloaded to the EVM easily through Haptic Control Console. Editing…
Part Number: DRV2511-Q1 Tool/software: Hi,
Datasheet has a table about frequences when PWM signal < %96. I set the FS2 = 0, FS1 = 0, FS0 = 0 and my oscillator frequency is 400 Khz.
I want to see no output when When i applied logic 0 to input …
Part Number: MSP-EXP430G2ET Other Parts Discussed in Thread: DRV2511-Q1 , Hi Sirs
Goal: Develop solenoid driver TI DRV2511-Q1 with TI MCU Lunch Pad with Code composer studio
Prepared: TI Launch Pad kit(MSP-EXP430G2ET), DRV2511-Q1 EVM kit, USB2UANY…
Part Number: DRV2511-Q1 Other Parts Discussed in Thread: DRV2605 , DRV2625 If end customer want to deploy DRV2511-Q1 commercially, and they will tune some waveforms to support different user cases.
Will this total solution violate the immersion license…