Part Number: DRV2605 Other Parts Discussed in Thread: DRV2603 , DRV2603EVM-CT Hi Guys
Our customer wants to use our DRV2605, there are a few of questions below:
1. The motor used by the customer is a dual axis instead of a single axis. Can we support the…
Other Parts Discussed in Thread: DRV2603 , DRV2603EVM-CT , BQ25121 , DRV2604 , DRV2624 , DRV2604L I have a BLDC vibration motor, this one >> https://www.precisionmicrodrives.com/product/908-100-8mm-brushless-vibration-motor-3mm-type and I'm trying to drive…
Other Parts Discussed in Thread: DRV2603 , DRV2603EVM-CT , DRV2604L , DRV2605L Hello,
The EVM for the DRV2603 has a mode to turn off the autoresonance for an LRA motor. However, we don't see in the datasheet how to do that in our design. How do you turn…
Yaita-san,
The length of the cable should not be an issue. We typically test with wires that are longer in our lab, >50cm.
To test if performance is okay, please compare the waveforms in the DRV2603EVM-CT User's Guide with waveforms taken on the customers…
Lindsay,
In the DRV2603EVM-CT User's Guide, there is a short firmware programming section. It lists the part number from Digi-Key and Mouser. See snippet below.
Digi-Key: http://www.digikey.com/product-detail/en/850-10-050-20-001000/ED8650-ND/2…
Toso,
Thanks for looking at the DRV2603. Here are my recommendations:
The DRV2603 requires a GPIO and PWM pin to operate. If you need to operate 10-20 DRV2603, makes sure both of these pins are available for each device.
For layout, I would recommend…
Other Parts Discussed in Thread: DRV2603EVM-CT , DRV2603 I am running an MSP430 Launchpad to drive a DRV2603EVM-CT RevD CapTouch board.
I need to essentially build a shell to control the CapTouch board's actuators from my PC.
I have been scanning the…
Jake,
The DRV2603 NC pins are not connected internally to the die, so they can be left disconnected without issues. See the DRV2603EVM-CT layout for an example.
Thanks, Brian
Other Parts Discussed in Thread: DRV2603 , DRV2603EVM-CT , MSP430G2553 , DRV2604 , DRV2605 Hi,
I searched in the datasheet but did not manage to find the maximum output current of DRV2603. My application is about driving an ERM motor (307-002 cylindrical type…