Richard,
let's separate the issue
1. C17 on the USB-ISO connector of the TMDSHVMTR r1p1 kit
I agree, on first inspection this looks like an issue if you are using the USB-JTAG on the HVKIT. Let me send this to the owner. The good news is that you…
Other Parts Discussed in Thread: DRV8312 , CONTROLSUITE , DRV8301
I'm working with the BLDC_Sensored example for the DRV8312 kit. Here's some code from "f2803xbldcpwm_BLDC.h". It looks like it has multiple bugs (unless I'm missing something).
1. Why…
Hi,
I'm experience some strange behavior when using the graph tool in CCS v5.3. I'm running the DRV8312-C2-KIT to evaluate the control performance with steep ramps. In the attached graph I've plotted (using the exported data) the speed reference (target…
shailesh,
There is quite a lot of information, so I can understand being confused about www.ti.com/instaspin
Regarding the software architectures, this link should be helpful.
My advice is to learn InstaSPIN-FOC & InstaSPIN-MOTION in the following…
Other Parts Discussed in Thread: DRV8312 , CONTROLSUITE I have the DRV8312 kit and F28069 ISO controlCARD for testing new code. I have been trying to program timer 1 for 50 us intervals but I am getting 65-70 us. How can I improve timer accuracy?
…
Other Parts Discussed in Thread: MOTORWARE I work with kit DK-LM4F-DRV9312 and use an application "InstaSPIN™-BLDC Sensor less control for the Stellaris LM4F2x" Version 1.0.2. The CCSv5 was downloaded, installed, and i running.T hen the InstaSPIN project…
Other Parts Discussed in Thread: LAUNCHXL-F28027 Dear all,
While flashing the sensorless bldc code in f28035 card on DRV8312 kit i'm receiving the following error.
Kindly help me to rectify it. It also showed another error like the code was generated…
Part Number: LAUNCHXL-F28069M Other Parts Discussed in Thread: DRV8301
I've been trying to run a PMSM pump motor with the LaunchpadXL F28069 and BoostXL DRV8301 driver set for several days now, but so far unsuccessfully. I worked through the InstaSPIN…
Paolo,
in controlSUITE the DRV8312 and DRV8301 kits are dual built for F2803x and F2806x (I beleive NOT using the FPU).
There is also MotorWare. While this supports InstaSPIN-FOC and InstaSPIN-MOTION solutions - which requires special versions of…
Hey ET,
I was unable to find any docs for the F28069 ISO Control Card (CC) on my first look as well. I've never actually used that CC, but I would assume the differences between F28035 and F28035 ISO would be similar to what you would see for the F28069…