Hi Zied,
Just following up on this thread and wanted to ask if this inquiry is still open?
If so, please help to provide the above information. I will close this thread until further info is provided which will open the thread again.
I look forward to…
Hi Zied,
I cant really figure out what is wrong with your SPI read and writes. Let me share some of our code that we use with our devices to communicate via SPI
void Config_evm_spi(void)
{
//Pin Config
EALLOW;
// SPI_MOSI
GPIO_SetupPinOptions…
Part Number: DRV8323R Tool/software: I am planning to configure the DRV8323RS through SPI communication without using the CAL pin.
The CAL pin is internally pulled down in the IC (externally floating).
Is it possible to configure it through SPI regardless…
Part Number: DRV8323R Tool/software: I use the DRV8323RS and would like to know the minimum current flow in Vm. Since in the datasheet there is only typical (10,5 mA) and maximum value (14 mA) given, i ask here whether there is more information about…
Hi Morris,
Did you check the link Allison posted?
https://e2e.ti.com/support/motor-drivers-group/motor-drivers/f/motor-drivers-forum/1267198/boostxl-drv8323rs-i-want-to-know-the-parameters-of-this-inverter
It seems like all the parameters you are looking…
Part Number: DRV8323R Tool/software: Hi Team,
Previously, the DRV8323RS chip was used, with upper tube source/sink currents of 440mA and 380mA, and lower tube source/sink currents of 330mA and 280mA, respectively. It was used to drive a single MOS and…
In case its of any help, I have captured scope traces of the phase voltage and current when running lab 2 which causes the moduleOverCurrent fault.
Phase A voltage and current
Phase B voltage and current
Phase C voltage and current
Phase ABC voltage…
Hi Deven,
Apologize, I missed your reply.
For the guidance, I do NOT have bandwidth to do this, sorry...
While you could refer below documents to see how I do the migration on the DRV8323RS, it is expected to be similar and might be helpful for you migration…
Part Number: TMS320F280025-Q1 Tool/software: I am running 12.xx CC on a LaunchXLF280025C/DRV8323RS_A platform, running a sensorless/foc induction motor (15A max). motor control 4.0.xx labs 1 through 4 fun fine. I am bringing up a new PCB design with…