Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: DRV8662EVM Hello,
Hope you are well. I've previously asked about connecting multiple actuators for the DRV8662EVM, and the suggestion was to use FETs to switch between actuators. ( https://e2e.ti.com/support/other_analog/haptics/f/927…
Part Number: DRV8662EVM Other Parts Discussed in Thread: DRV2605LEVM-MD , , DRV8662 Hello,
I hope you are well. I am looking for a haptic driver that can actuate multiple piezo actuators and switch around actuators. I am currently using the DRV8662EVM and…
Part Number: DRV8662EVM Other Parts Discussed in Thread: DRV8662 Tool/software: Code Composer Studio Hello,
I recently adapted the main.c code of the MSP430 using CCS, so that the number of cycles (g_cycles) is around 50 and the frequency (g_bin) is lower…
Part Number: DRV8662EVM Other Parts Discussed in Thread: MSP-FET , DRV8662 , DRV2667EVM-CT , DRV2667 Hi Kelly,
Hope you're well. I have two questions about the DRV8662EVM. The first is about changing the waveform frequency. I know that the MSP430 can…
Other Parts Discussed in Thread: DRV8662EVM , DRV8662 I'm attempting to use the DRV8662EVM. Unfortunately, it either isn't delivering what the spec says it should deliver, or I'm doing something wrong. I suspect the latter..
Anyway, I want to…
Other Parts Discussed in Thread: DRV8662EVM I've hooked up a DRV8662EVM to a 5 volt power supply and an external analog sine wave signal of 1.8 volts, peak to peak, with a frequency of 10 hz. however, when I set the gain to 34 via TRG button, which should…
Thank you for the feedback - "I suspect something is damaged somewhere along the signal chain" - TI suggested the same thing but want to confirm - you replaced C4 & C5 with a 0-Ohm short to the input of U1 then applied Vdd/2 to offset the input…
Part Number: DRV8662 Hi team,
DRV8662‘s output is normal on condition of no p iezo load, but output abnormal with piezo load
Attached are the waveform with and no piezo load!
SCH is same to the DRV8662EVM schematic
piezo load is 3.7uF
Gain1=Gain2=0 …
Other Parts Discussed in Thread: DRV8662EVM Downloaded the DRV8662EVM Source Code (sloc285.zip) file from the DRV8662EVM product page, and it expanded to a DRV8662EVM_RevD folder. Looks like the code is configured for the IAR MSP430 IDE, not CCS.
Anybody…