Part Number: DRV8801-Q1 Hi team,
In the process of forward and reverse rotation, how to judge that it has rotated to the specified position? Will IC have a feedback signal?
BR,
Jimmy
Part Number: DRV8801 Hi team,
thanks for your support before.
We know that when DRV8801 in sleep mode, then we don't care nFault PIN as datasheet said below.
but my customer's test standard that need float current <1mA, but some DRV8801 (which…
Hi Can,
What I found digging through other e2e posts is the VPROPI output should be ignored when ENABLE is low because the internal amplifier is in an undefined state. This is the thread that explains what you're seeing (towards the bottom): https:…
Part Number: DRV8801 Hi Team
There is a good new that we DIN DRV8801PWPR !
At present, customer uses DRV8801PWPR. If the Pin 1 function is not used, can Pin 1 be directly grounded? If not, can R29 be increased to 100K?
Part Number: DRV8801
Hi experts,
Before we start to put this to a prototyping project, my IQC observed copper marks on the pins.
Because we only have limited pieces for use, please advise what are these marks and if it will affect usage.
/resized…
Hi Ikeda-san,
The device is tested for 50kHz. Typical motor driver applications are not designed for frequencies of the magnitudes you specify.
The DRV8412 and DRV8432 are designed for PWMs up to 500kHz, have better Rdson, dead time, and propagation…
Part Number: DRV8801 1. How to adjust the duty cycle to 100%? Is it enable pin? 2. In order to reduce the current ripple, what is the recommended value for the motor series inductance? 3. Select 0.3ohmItrip=1.67A If the current is 1.2A VPROI=5 x I I…
Part Number: DRV8801 Other Parts Discussed in Thread: DRV8828 , Hi Team,
Our customer is looking for an H-Bridge motor driver for a 12V, 0.5A BLDC water pump motor. I have attached the details of the pump below. Upon checking our product lines, the…
Part Number: DRV8801 Other Parts Discussed in Thread: DRV8876 Hello Guys,
Good day.
Our customer is looking to use DRV8801 on his project.
Can DRV8801 drive this motor? https://www.maxongroup.com/maxon/view/product/motor/dcmotor/re/re13/118464 …
Part Number: DRV8801 Hello everyone !
I am currently working on integrating a DRV8801 into a design for driving a low-impedance, brushed DC motor at around 12V. I would like to use the VpropI output to get current readings but I have been unfortunate…