Part Number: DRV8833 Hi Team,
The electric motor driver has no load. The input at AIN1 is 0V, and that at AIN2 stands at 20KHZ. The duty cycle is 40%, and the square wave has an amplitude of 3.3v as shown below.
The yellow line in the figure stands for the…
Part Number: DRV8833 Hello:
The schematic diagram of intelligent door lock project. Please check the drv8833 circuit currently used to see if there is any problem. thank you
Part Number: DRV8833 Hello.
Could you ask us a question about the Motor Driver IC (DRV8833)? As we evaluate the motor driver IC, the connection terminals with the motor (AOUT and / AOUT2) are applied to the back electromotive power by about -1V when the…
Part Number: DRV8833 Excuse me many times, but let me ask you additional questions.
Please tell me about the soldering conditions of DRV8833.
that's all, thank you very much.
Part Number: DRV8833 Let me ask you about the plating of the terminals.
Is it correct that the plating material for the terminals of the DRV8833PWPR is Sn?
I saw an article that all the terminal plating of TI's products is Sn, but I can not confirm it…
Part Number: DRV8833 I need to drive one of the IN inputs high but when connecting it to the VM supply, I may exceed the 7 volts input max limit. Can I connect it to VINT instead?
Part Number: DRV8833 Hello. I am using DRV8833 for low voltage motor. In my circuit, I only use the reverse. I don't use PWM. Now I have a question about keeping the engine speed constant. It's like old cassette recorders. It used an electronic circuit…
Part Number: DRV8833 Hello.
What are the storage conditions, storage period and baking conditions for unopened and opened in a package DRV8833?
Thank you .
Part Number: DRV8833C Other Parts Discussed in Thread: DRV8833 , Hi,
Good Day. I have a customer who is working with DRV8833/C. Please see below his query for your reference. Thank you very much.
I am interested in using both DRV8833PWPR and DRV8833CPWPR…