Part Number: DS100BR111 Tool/software: Hi,
Plan to use DS100BR111 as a repeater for 10G-SFi, what should be the configuration on Mode pin (18) for 10G SFI
Part Number: DS100BR111 Other Parts Discussed in Thread: DS100BR210 Tool/software: Our intent is to use the device in the SMBus Master Mode (ENSMB = Float) to read in device setup values from an external EEPROM at power-up. However, section 8.3 SMBus…
Part Number: DS100BR111 Tool/software: I successfully installed SigCon with RTE v3 (snlc066b.zip) but when I try to run the DS100BR111 profile updater from snlc056a.zip I get the following error:
Do I need install the older version of SigCon in order…
Part Number: DS100BR111 Tool/software: We plan on using the DS100BR111 configured as a 10G-KR repeater. We are getting into SI analysis of the design and have the following questions:
JITTER
Typical deterministic jitter values (DJxx, see Nov2014 datasheet…
Part Number: DS100BR111 Tool/software: I´m looking for best option on 10Gb ethernet, which are the recommended redriver for 10GBASE-KR and 10GBASE-KX ?
Thanks!!!
Part Number: DS100BR111 Other Parts Discussed in Thread: DS110DF111
Hi, I would like to ask if the DS100BR111 redriver would be appropriate for supporting 10GBASE-R interfaces at an SFP+ port?
The 10 GBe signals are 10GBASE-KR from a 3U VPX general purpose…
Part Number: DS100BR111 Please confirm that the DS100BR111 is more appropriate than the DS100BR111A for use with a 10GBASE-KR link (with link training on). We would also like to use the same part for a 1000BASE-KX link. I had noted that previous forum…
Part Number: DS100BR111 Other Parts Discussed in Thread: DS100DF410 , DS280MB810 In our design, Lane Repeater (DS100BR111SQE/NOPB) going to use up to 10.3Gbps data speed. Is power supply noise will be impact the performance of this IC ? If it will be impact…
Part Number: DS100BR111 Hi team,
I saw that this part has +36dB Receive Equalization and -12dB Transmit De-emphasis. Does -12dB De-emphasis have the equal effect with +12dB Equalization to the same channel? We tested the 10Gbps data BER of one lossy channel…
Part Number: DS100BR111 Team,
For 10G operation the datasheet SNLS338F specifies at page 31 that Register 0x08 register bit 3 need to be set to 1:
-What is then the procedure to enable manually the different channels? -Do you have some kind of register…