Part Number: DS160PR410 Other Parts Discussed in Thread: DS100BR210 , DS64BR111 , DS100BR111 Tool/software: We are thinking of using either the DS64BR111 and DS100BR210 part for our board design. Our biggest question will be availability and lifetime…
Part Number: DS100BR210 Hello,
I am trying to run a signal integrity check in hyperlynx that uses the DS100BR210. I have setup the model correctly however from your datasheet I am having trouble understand eye width and height requirements at the…
Part Number: DS100BR210 Hello, We are using the DS100BR210 in 10G-KR Mode. (Back-plane) It is configured as follows: ENSMB = 0 (Pin Mode) VOD_SEL = 1 (10G-KR Mode) VDD_SEL = 0 (3.3V Operation) MODE = 1 (10GbE Mode, Continuous Talk) TX_DIS = 0 (OUTA and…
Part Number: DS100BR210 Other Parts Discussed in Thread: DS100BR410 , Hi team,
There are 3 questions need your help:
1. for DS100BR210 CML receiver input level Vtx, where is the differential measurement point? Is it same as TPA in DS100BR410 datasheet…
Part Number: DS100BR210 Hi Team,
Our customer is looking for the Recommended Operating Junction Temperature (Tj) of the DS100BR210SQ/NOPB. According to our customer,
In particular, I’m looking for:
the Recommended Operating Junction Temperature…
Part Number: DS100BR210 Other Parts Discussed in Thread: LMH1218 , LMH1219 , Hello,
In our application, we need to support both SMPTE 292 video input and output. So we plan to use both LMH1219 and LMH1218 for this application. The FPGA and the LMH1218…
Part Number: DS100BR210 Hi all,
I am looking for some additional information regarding the DS100BR210 thermal characteristics, namely the following:
1. Recommended Operating Junction (Tj) or specifically the temperature at which full functionality…
Part Number: DS100BR210 My requirement is to connect the RJ45 interface of a PC to a network switch with a redriver unit between them. I tried using DS100BR210 but realised that it works only with 10G-KR. Is there any similar IC available which works…
Part Number: DS100BR210 Can I use this IC for 1000 Base-T application? My requirement is to connect the RJ45 interfaces between 2 PCs (in cross fashion) with a redriver unit between them.
Part Number: DS100BR210 I'm planning to use DS100BR210 for isolating the network interface of a PC (100 Mbps) upon receiving a digital signal. I tried the basic pin mode control (ENSMB = 1kOhm to GND) with EQ and DEM set to 0 and VOD_SEL set to 1. MODE…