Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: DS100BR410 Tool/software: Hello, I'm in the process of choosing an Equaliser where I require x5 channels supporting a data rate up to 3.2Gbps. In my initial search this part appeared to be a potential contender, though the datasheet lacked…
Hi Lucas,
TKS for your reply. About the issue of p eak-to-peak signal amplitude and the eye height.I have two question:
1 If i need to evaluate the signal@ input pin of DS100BR410.How to evaluate the closed eye diagram whether meet the requirement of DS100BR410…
Hi Rick,
From TI side, there is no preference to use 3.3 V or 2.5 V supply mode. In 3.3 V mode, an internal LDO regulator is used to step the supply down to 2.5 V internally.
A DC-to-DC converter can be used for the 2.5 V supply as long as it meets datasheet…
Part Number: DS100BR410 Tool/software: What is the recommended replacement part for a Gen2 PCIe application? Is it the DS100BR410SQE/NOPB or is there a better choice?
Part Number: DS100BR410 Tool/software: Good afternoon,
What are the main performance differences between the three PNs listed in the thread title? I see that the 401 and 800 devices each have 8 channels where the 410 only has 4 and I noticed the pinouts…
Part Number: DS100BR410 Other Parts Discussed in Thread: DS100BR111 , DS100BR111A
Hello,
I have a on board chip to chip connection with 10G SFI to 10G XFI(no optical modules involved), due to the long trace I would like to use DS100BR410 in the middle…
Part Number: DS100BR410 Tool/software: Good morning,
Is it acceptable to leave the SDA, SDC, and CS pins on the DS100BR410 device not connected when I have the component set to pin control mode? On the datasheet it has a note that says external pull…
Part Number: DS100BR410 Is it possible to read from a DS100BR410 register or registers the state (high or low) for the BST pins-
BST_2 = Pin 37
BST_1 = Pin 14
BST_0 = Pin 23
For example, can the state of these pins be read from the "Status Register for…
Part Number: DS100BR410 Hello expert,
May I know if DS100BR410 or other 10G retimer/redriver can support SGMII TX/RX? If yes, could you provide suitable solution for us? If no, which device is more suitable for SGMII? Per checked with SGMII spec, it can…
Part Number: DS100BR410 Hello.
I have a question about the Boost / EQ SMBus Register on the DS100BR410.
On page 14, table 5 of the datasheet, there is a register for setting the gain in SMBus, but what if I want to set 16 levels in more detail?
The register…