Part Number: DS100BR410 Is it possible to read from a DS100BR410 register or registers the state (high or low) for the BST pins-
BST_2 = Pin 37
BST_1 = Pin 14
BST_0 = Pin 23
For example, can the state of these pins be read from the "Status Register for…
Part Number: DS100BR410 Hello expert,
May I know if DS100BR410 or other 10G retimer/redriver can support SGMII TX/RX? If yes, could you provide suitable solution for us? If no, which device is more suitable for SGMII? Per checked with SGMII spec, it can…
Part Number: DS100BR410 Hello.
I have a question about the Boost / EQ SMBus Register on the DS100BR410.
On page 14, table 5 of the datasheet, there is a register for setting the gain in SMBus, but what if I want to set 16 levels in more detail?
The register…
Part Number: DS100BR410 Other Parts Discussed in Thread: DS50PCI401 , DS50PCI402 We are using the DS100BR410 for a cabled PCI express (gen1) application as replacement of the DS50EV401SQ/NOPB (which is EOL).
we run into the issue that the link is not established…
Part Number: DS100BR410 Hi team,
My customer is setting up the EQ gain by reffering to the Table 5 on the datasheet. It looks like there are 16 patterns for EQ gain. My customer would like to set EQ gain step by step like 1dB, 2dB, 3dB etc.. Do we have…
Part Number: DS100BR410 Please let me know about POWER SUPPLY BYPASSING for the DS100BR410.
On page 15 of the datasheet, it states that three capacitors with capacitance ranging from 2.2µF to 10µF should also be incorporated in the power supply bypass…
Part Number: DS100BR410 Please let me know about SMBus function of DS100BR410.
In page 10 of the datasheet, it says that the SMBus port is enabled when the CS pin of the SMbus is set High.
If I2C communication is used only with the DS100BR410, can the…
Part Number: DS100BR410 Please let me know about SMBus function of DS100BR410.
In page 10 of the datasheet, it says that the SMBus port is enabled when the CS pin of the SMbus is set High.
If I2C communication is used only with the DS100BR410, can the…
Part Number: DS100BR410 Other Parts Discussed in Thread: DS100MB203 ,
Hi team,
A customer is considering development by using Repeater DS100BR410 and MuxBuffer DS100MB203. There is a description that slave management bus interface of both device is compativle…
Part Number: DS100BR410 Hi, I have three questions about the features of DS100BR410.
(1) When PIN_MODE pin is connected to GND and fixed to Low, is it OK to leave BST_0-BST_2 pins open?
(2) If the SIGNAL DETECT function is not used, is it OK to leave…